This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 kernel make error messages...



hello:

i added a new machine item in arch/arm/mach-davinci/Kconfig and configure "menuconfig".

(also add it in mach-type)

then i make my new kernel,there are 2 error messages as below:

1.:no machine record defined

2.fs/built-in.o: In function `cramfs_fill_super':
  file.c:(.text+0x74c1c): undefined reference to `get_mtd_device'

 

for error 1:

i have set all realte with ti-davinci options of "System Type--->" in menucoufig .

for error2:

i have include the header which declare the called function, but compiler still shows "undefined reference.."

now i have no idea to solve, ... do i miss sothing???

can any one teach me..thank you very much^^( forgive my bad english..)