Hi,
I am running fatfs console test example to communicate with eMMC on SK-TDA4VM board using processor SDK RTOS version 08_06, when I run the code, eMMC initialization is getting failed.
The above piece of code is in MMCSD_v2_initEmmc function of file MMCSD_v2.c, when this command is transferred, I am getting COMMAND EXECUTION FAILED error in the MMCSD_v2_transfer function.
There is no code change I am just running the example code in SDK and it is not running. Please support me to resolve this issue.