This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to import matrix_tui



Dear Sir

I want to work with the AM37xx processor.

I followed all the steps from the beginning

1. Installing CodeSourcery Lite

2. Installing the AM37x SDK

3. Setting up Minicom in Ubuntu

4. Modifying U-boot

5. Code Composer studio v5 Preview Edition Users Guide

       i. How to start Code Composer studio v5

       ii. How to import QT Projects into CCSv5

       iii. How to Run GDB on CCSv5

                                        And i got stuck while

doing this step

       iv. Setting up the CCSv5 on the Host

i could not get the matrix_tui and dhrystone on the Project window.

(I did not install Bluetooth and WLAN)

Kindly help me in this issue.

regards

Joel Josephson P

  • Hi Joel,

    Can you verify which Software Develompent Kit (SDK) you have downloaded. Is it 4.0 for AM37x?

    Please consider downloading the latest SDK for AM37x SDK 05.02.00.00. It may not fix your issue, but it is two releases beyond what you are using. Also there are many more sample applications and a newer toolchain that comes with SDK.  Also it contains a later version of the Linux kernel - 2.6.37.