Other Parts Discussed in Thread: OMAP3530
Hi All
Apologies for the partial posted message earlier on this subject (had problems with cookies ..:)
Trying to migrate a CCS3.3/XP/EVM based project to CCS4.2/windows 7/eXperimenter.
The sample BSP projects appear to work OK on the eXperimenter but when I try to build the "Import legacy CCS3.3 project" get a number of errors which are usually resolved by adding appropriate include paths.
However when looking for a _hal_cache.h file path the only instances of this file are contained in directories (../dsplink/dsp/src/base/hal/DspBios/<directories>) where the directory names are not an obvious match for the eXperimenter (the listed directories are DM648, DM6437, OMAP3530 ...)
Have I missed a step in my installation that may cause this ? If so is there a way to correct the issue without risking corrupting the already installed software packages ?
BR
Barry