This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

power pins used in the DM8148 EVM and are not mentione in the DM8148 datasheet

4336.u27p_centarus_EVM.doc

 

in the centaurus EVM the are power pin that are connected to the supply/GND (see doc)

does pins are mentione as NC in the DM8148 datasheet

are does pins used of future options in the EVM ?

if i do not connect does pins is ok by TI?

 

regards

pablo

 

 

  • Pablo,

    The extra power and ground pins connected in the schematics (U27P) are for TI internal test purposes.  The chips that are shipped to customers do not have these balls populated on it.  The data sheet is correct, the extra pins used in the schematic should be left as no-connects.

    Anytime there is a disagreement between the data sheet and the EVM, the data sheet rules.

    Best regards,
    Scott