Part Number: AM625
Hello Team,
Posting on behalf of mu customer:
I need specific information about the AM625 series, it has a M4 co-processor.
Is the GPU dependent on the use of the coprocessor or is it independent of its resources and operations?
1. I wish to know if the co-processor has specific duty assigned to it, like assisting GPU with load or other functions.
2. If I can run a separate runtime on the co-processor for example, Open PLC runtime and install Linux to run exclusively using the main processor and using the coprocessor dedicated to the particular task?
3. If possible, how do I make it work with the firmware or Linux kernel, and If not what other TI MPU allows me to get this exact functionality?
Regards,
Renan