Hi,
Can the C6748 support both ADC and DAC using the uPP ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can the C6748 support both ADC and DAC using the uPP ?
Hi Said,
I moved your post to its own thread because it did not fit in the C6747 ADC thread.
To answer your question, yes the UPP supports both ADCs and DACs. From the UPP description in the datasheet:
The Universal Parallel Port (uPP) peripheral is a multichannel, high-speed parallel interface with dedicated data lines and minimal control signals. It is designed to interface cleanly with high-speed analog-to-digital converters (ADCs) or digital-to-analog converters (DACs) with up to 16-bit data width (per channel). It may also be interconnected with field-programmable gate arrays (FPGAs) or other uPP devices to achieve high-speed digital data transfer. It can operate in receive mode, transmit mode, or duplex mode, in which its individual channels operate in opposite directions.
Thanks Tim for your reply,
The problem is that this DSP TMS320C6748 is new but very interesting because he offers many externals peripherals.
I did some research to interface The ADC and The DAC to the DSP with a daughter board but I didn't find.
Thanks,
Said Dorgaa