Part Number: AM625
Dears,
Pls kindly help to check whether the am6254 can support the MIPI CSI such as IMX415&IMX335 or not?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM625
Dears,
Pls kindly help to check whether the am6254 can support the MIPI CSI such as IMX415&IMX335 or not?
Thanks
Hello Ning Li
Thank you for the query.
Are you checking if we have tested or the feasibility to use.
Please refer the below section of the datasheet for information on the CSI interface and should connect to any device supporting the below CSI capabalities.
Table 6-7. CSIRX0 Signal Descriptions
One Camera Serial interface (CSI-Rx) - 4 Lane
with DPHY
– MIPI CSI 1.3 Compliant + MIPI-DPHY 1.2
– Support for 1,2,3 or 4 data lane mode up to
1.5Gbps
Regards,
Sreenivasa
Hi Sreenivasa,
Yes,I want to know the am625 can support IMX415,IMX335?
Thanks
Hello Ning Li
Thank you for the inputs.
Please refer data sheet and TRM for the supported CSI interface.

On a theoretical basis, AM625 should be able to support any sensor that supports the CSI-2 interface.
Ex for imx335:

We have tested the OV5640 but do not have any information on having tested the above sensors.
Regards,
Sreenivasa
Hello Ning Li
Pls refer additional inputs:
You can check the drivers for those sensors in linux upstream to see what link freq it uses and what data rate (link freq * 2) AM62x CSI-2 interface is advertised to support
https://github.com/torvalds/linux/blob/master/drivers/media/i2c/imx415.c#L113
https://github.com/torvalds/linux/blob/master/drivers/media/i2c/imx335.c#L52
Refer below for the AM62x documentation
FYI, Refer below for the AM62A documentation
Regards,
Sreenivasa