Other Parts Discussed in Thread: SYSCONFIG
All,
I currently have an issue setting up an interrupt on the OMAP 3530 IVA module(a.k.a DSP) . I am trying to use GPIO 22 and 23 for the interrupt. I first configure the appropriate padconfig register to Mux_Mode_4 and input enable
// gpio 22
pSTBCtx->Hardware_Context.pPadConfig->CONTROL_PADCONF_ETK_D8=(MUX_MODE_4|INPUT_ENABLE);
// gpio 23
pSTBCtx->Hardware_Context.pPadConfig->CONTROL_PADCONF_ETK_D9=(MUX_MODE_4|INPUT_ENABLE);
I then setup the bank 1 registers as shown below
#define GPIO_22_BIT_OFFSET (1<<22)
#define GPIO_23_BIT_OFFSET (1<<23)
#define SCHEDULE_REQUEST GPIO_22_BIT_OFFSET
#define COLLECTION_DONE GPIO_23_BIT_OFFSET
pSTBCtx->Hardware_Context.pBank1->OE|=SCHEDULE_REQUEST|COLLECTION_DONE;
pSTBCtx->Hardware_Context.pBank1->RISINGDETECT|=SCHEDULE_REQUEST|COLLECTION_DONE ;
pSTBCtx->Hardware_Context.pBank1->SETIRQENABLE2=SCHEDULE_REQUEST ;
pSTBCtx->Hardware_Context.pBank1->SETIRQENABLE2=COLLECTION_DONE ;
At this point I see the following in the Bank registers.
pBank1 0x48310000 OMAP_GPIO_REGS * hex NotEdited
REVISION 0x00000025 REG32 hex NotEdited
zzzReserved01 0x48310004 unsigned int[3] hex NotEdited
SYSCONFIG 0x00000015 REG32 hex NotEdited
SYSSTATUS 0x00000001 REG32 hex NotEdited
IRQSTATUS1 0x00400000 REG32 hex NotEdited
IRQENABLE1 0x00000000 REG32 hex NotEdited
WAKEUPENABLE 0x00000000 REG32 hex NotEdited
RESERVED_0024 0x00000000 REG32 hex NotEdited
IRQSTATUS2 0x00400000 REG32 hex NotEdited
IRQENABLE2 0x00C00000 REG32 hex NotEdited
CTRL 0x00000000 REG32 hex NotEdited
OE 0xFFDE3FFF REG32 hex NotEdited
DATAIN 0x000100BC REG32 hex NotEdited
DATAOUT 0x00010000 REG32 hex NotEdited
LEVELDETECT0 0x00000000 REG32 hex NotEdited
LEVELDETECT1 0x00000000 REG32 hex NotEdited
RISINGDETECT 0x00C00000 REG32 hex NotEdited
FALLINGDETECT 0x00000000 REG32 hex NotEdited
DEBOUNCENABLE 0x00000000 REG32 hex NotEdited
DEBOUNCINGTIME 0x00000000 REG32 hex NotEdited
zzzReserved02 0x48310058 unsigned int[2] hex NotEdited
CLEARIRQENABLE1 0x00000000 REG32 hex NotEdited
SETIRQENABLE1 0x00000000 REG32 hex NotEdited
zzzReserved03 0x48310068 unsigned int[2] hex NotEdited
CLEARIRQENABLE2 0x00C00000 REG32 hex NotEdited
SETIRQENABLE2 0x00C00000 REG32 hex NotEdited
zzzReserved04 0x48310078 unsigned int[2] hex NotEdited
CLEARWAKEUPENA 0x00000000 REG32 hex NotEdited
SETWAKEUPENA 0x00000000 REG32 hex NotEdited
zzzReserved05 0x48310088 unsigned int[2] hex NotEdited
CLEARDATAOUT 0x00010000 REG32 hex NotEdited
SETDATAOUT 0x00010000 REG32 hex NotEdited
zzzReserved06 0x48310098 unsigned int[2] hex NotEdited
As you can see the IRQSTATUS2 indicates that the GPIO 22 has triggered.
I now enable the Wugen with following call
#define EVENT_ID_BANK_1 73
HWI_enableWugen(EVENT_ID_BANK_1);
I read the WUGEN_MEVTSET1 register below:
0xEFFFFFFF
This indicates that IRQ 28 is unmasked(I think). However when I read the WUGEN_PENDEVT0 register. I get:
0x00008000
I think the value should be 0x1xxxxxxx.
I then map the event to an interrupt:
#define HWINT_BANK6 7
HWI_eventMap(HWINT_BANK6,EVENT_ID_BANK_1);
I then Plug the ISR
//The ISR needs to be plugged
HWI_dispatchPlug(HWINT_BANK6,Gpio_Bank6_ISR,-1,NULL);
Finally I enable the IER
//The corresponding IER bit needs to be enabled.
C64_enableIER(1<<HWINT_BANK6);
But I never see the ISR get called and the corresponding bit in the IFR never gets set.
Any ideas?
Thanks,
Ram