Now, I am using EMIFA of C6747 to read a 16 bit FIFO. When I configure the EMIFA working on 16-bit data bus mode(ASIZE = 1h) to read the FIFO, I miss one data every two data. For example, what I should get is 0,1,2,3,4,5,6,7,8, but I get 0,2,4,6,8 instead. I checked the CS and OE signal via an osciliscope, and find that there are two OE low pulses in each low period of CS. When I config the EMIFA working on 8-bit data bus, I find that there are four OE low pulses in each low period of CS. I guess this is because of C6747 is a 32-bit CPU. But I find EMIFA of C6747 does not support 32-bit data bus.
I just wonder how can I use EMIFA to interface with a 16-bit FIFO without missing any data?
Thanks for helping!