Hello,
I would like you to confirm whether you have confirmed about below or not.
* According to schematic of SK-AM62, there is no device which can be controled by McSPI on SK-AM62.
To confirm McSPI function, user need to connect certain device to EVM via expansion connector ("J3" connector of EVM).
Then I have following question.
Q, Have you ever had any experience which you connect something SPI device via expansion connector("J3" connector) to confirm behavior of McSPI function on SK-AM62 under linux ?
If answer is yes, could you please tell me which device(parts number) you have connected ?
Best Regards,