hi all i (i m using dsj6713 and ccs v3.1) have made a c file by coping it from rulph chasaing book the c file contains the instructions to turn led '0' on when diop switch '0' is pressed and to output tone on the line out or headphone output of dsk.i have also added all the necessary files in the project as mentioned in the book.now when i run th eproject the led '0' does blink in accord with the programme but the tone appears after several number of rebuilds and it may disappear if i rebuild it just once more after getting it.has anybody encountered this problem or have some idea how to solve it i m waiting for your reply.
Mateen