This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: CAN Send-Receive Data Issue

Part Number: SK-AM62

Hello E2E Experts,

Good day.

The CAN can't send and receive data:

root@am62xx-evm:~# ip link set can0 type can bitrate 1000000
root@am62xx-evm:~# ip link set can0 up
[ 79.081593] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready
root@am62xx-evm:~#
can0: flags=193<UP,RUNNING,NOARP> mtu 16 metric 1
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 42

Regards,

CSC