Part Number: TDA4VM
Hi team,
rtos_sdk: ti-processor-sdk-rtos-j721e-evm-08_01_00_13
linux_sdk: ti-processor-sdk-linux-j7-evm-08_01_00_07-Linux
Development Boards: custom board using the j721e chip.
The customer have done some development on muc3_0 and are now planning to port code for mcu3_0 to mcu1_0 (debug successful on CCS). Now try to start mcu1_0 with SPL. In the SPL boot, the storage medium is emmc. During debugging, it was discovered that the code for mcu1_0 was launched through the bootloader of a72 (tispl.bin), so the customer recompiled u-boot and burned tispl.bin from the a72 directory back into emmc:

However, the following error was found during reboot and the program gets stuck here:
They've also tried to rebuild tispl.bin with the code from mcu1_0 in the prebuild directory, and then reboot it, but it still cannot start:

Could you help check this case? Thanks.
Best Regards,
Cherry