Part Number: AM3354
Hi,
Customer would like to use USB0 with device mode and USB1 with host mode.
There are 2 questions.
1. How can it connected when use USB0 without VBUS from PC?
it will use only D+, D- and GND.
could you check below connection?
VBUS is floating and there is no pull up on D+

2. USB1 for host mode
USB1 is connected to LTE module and LTE module USB_VBUS is 1.8V.
Is USB available with only D+, D- connection to LTE module without 4.4V for USB1_VBUS?
or for host mode, is 4.4V mandatory on USB1_VBUS?
Thanks.