Hi,
I have a question for below three CPSW errata from my customer.
i2184 CPSW: IET express traffic policing issue
i2185 CPSW: Policer color marking issue
i2208 CPSW: ALE IET Express Packet Drops
It is not clear whether workaround is implemented in SDK8.6.
Suppose users setup environment based on AM64x EVM and the SDK, below commands cause these errata behaviors?
# > dhcp eth0
# > scp /boot/Image linux@192.168.20.188:~/
# > ping 192.168.20.50
If the answer is "NO", what makes these errata happen?
Thanks and regards,
Koichiro Tashiro