Is there a free, non-GPL USB example code out there?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a free, non-GPL USB example code out there?
Faraz,
I assume you mean for OMAP-L1x Processors?
There are a couple of options for you. You can download the free JUNGO USB Stack, though it's fairly complex and relies on closed source libraries. Takes some time to understand. At this time, other than the Linux Drivers we do not have any non-GPL USB example code specifically for OMAP-L1x processors.
You may to check out the Sitaraware Package. They have ported the Stellaris USB stack to the ARM9. Since the devices have similar architectures, you could also use this on the ARM side of the OMAP-L13x since both the AM1x and OMAP-L1x both have the ARM926 CPU core integrated into the silicon.