Hi,
I am using AM4376 processor and i have I have modified the EMACH switch example code in Myexampleproject folder in processor_sdk_rtos_am437x_6_03_00_106. I am able to use it as a switch in EMAC_Switch mode. but i am not able to assign IP address since I the device to be in Switch mode as well as should also have IP address to it along with MAC address.
Is it possible to implement in the above processing mode. since it is the requirement of our device. Please suggest regarding the same.
BR,
Gaurav More