Other Parts Discussed in Thread: TMS320C5515, ADS1298
Hi all,
we have a TMS320C5515 EVM and a ADS1298 ECG Daughterboard.
Connection to PC is via USB J11
When I start the ADS1298ECG-FE PC Software, it seems to attempt to download a Firmware, even though i cannot see any windows USB enumeration taking place.
The PC SW stops with:
The firmware load has failed due to a timeout condition......
As I saw here in the forum there is a windows 7 issue, but we use windows XP.
What firmware needs to be programmed into the EVM? Currently there is:
ads1298evm-pdk.bin
successfully programmed, I can see the 5515 EVM Demo dialogue on the OLED.
I just miss the evm connecting to windows as any USB device, or a driver installation.
Any hints?
Looking forward to any response,
best Regards
David