This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UPDATED: procmgrapp problem while loading 8168's M3s (for video subsystem bringup).



 

All,

We're seeing problems when attempting to load the dm816xbm_m3video.xem3 and dm816xbm_m3vpss.xem3

images onto the CortexM3s of an 8168 processor. We've been perusing the forums and have seen similar problems

reported by others but the problems/solutions don't quite match what we're seeing.

    UPDATE:

        Just came across another post on the forum where it was mentioned that the

        ti-ezsdk_dm816x-evm_5_01_01_80 SDK does *not* allow for changes in the memory map

        which would impact the CortexM3 functionality if boards have less than 1GB of memory.

        Can anyone confirm this? If that's true, is this being planned for the next SDK release (Aug?)

         to allow for alternatives to the fixed memory map? How will this be addressed for the *.xem3

         f/w images if that code will be closed-source (the video subsystem code)?

 

Specifically, we've built our Syslink drivers/apps and gotten our *.xem3 images from the ti-ezsdk_dm816x-evm_5_01_01_80

and have been able to get the *.xem3 images loaded on a C6A816x evaluation module from Spectrum Digital (the DDR2 model)

successfully. Though we can't run the full blown OmxInit examples on the older EVM we were able to at least load the M3s of

the C6A816x and insmod the relevant drivers (vpss.ko, ti81xxfb.ko, and TI81xx_hdmi.ko) with no problems so that we

could light up the frame buffers at the linux level (/dev/fb0,/dev/fb1,/devfb2) and check out the OnChip-HDMI.

 

When we use these same binaries on an alpha board using an actual 8168 (not the C6A816x) the procmgrapp

hangs and won't continue or allow itself to be Control-Z'ed  so we can't continue to work with the console. It hangs

on the Ipc_control(...) call when procmgrapp attempts to do the STARTCALLBACK.

 

# ./procmgrapp_debug 1 dm816xbm_m3video.xem3 0
ProcMgrApp sample application
Entered SysLinkSamples_startup
SysLinkSamples_osStartup
Entered ProcMgrApp_startup
ProcMgr_attach status: [0x0]
After attach: ProcMgr_getState
    state [0x1]
ProcMgr_load status: [0x3046000]
After Ipc_loadcallback: ProcMgr_getState
    state [0x3]
ProcMgr_start passed [0x6a85000]

#### hangs ....

 

We are using the recommended Code Sourcery Tool chain and don't encounter this problem with procmgrapp

when we attempt to load the DSP [we used the EZSDK syslink rtos samples to get an *.xe674 image for

comparison testing and the test ran fine].

 

So far it seems to be only an issue with loading the M3s on an 8168 and not with the other cores or on the

C6A816x.

Are there additional registers (PRCM/CLKs/etc) that need to be turned on if we're on an actual 8168 that

are being ignored on a C6A816x platform to load the M3s?   We're not trying to do anything fancy yet

(captures, encoding, etc) so we didn't expect to have differences yet for this range of board checkout/testing.

 

We've also tried using the Ducati() GEL file script from the Ti816x_ddr.gel file (and other related menu items) to

see if we could "poke it along"  just in case we missed something but that didn't help.

 

Any thoughts or suggestions? Is anybody else seeing this flavor of the problem [where even the Control-Z

workaround didn't work]?

 

Thanks in advance for any insight.

- Juan

  • Please run the prcm config tool which should set all the necessary clks

     

    http://e2e.ti.com/cfs-file.ashx/__key/CommunityServer-Discussions-Components-Files/717/1072.prcm_5F00_config_5F00_app


  • Hi Marcus,

    Thanks for the reply.

    We used the prcm app that came bundled with the EZSDK for our
    attempts on the EVM and on our ALPHA boards and it didn't complain
    or give any errors.

    But at this point we've got nothing to lose so we'll give this a
    try. I'm working off-site today but I expect to be back at my office
    tomorrow and I'll be sure to give this a try.

    Just to inform you that our ALPHA boards are right now setup with
    only 512MB RAM instead of the 1 GB memory map and I'd come across
    some postings that indicated that this wouldn't work [at least not yet
    with the current EZSDK because of the fixed memory map].

    I'll let you and the community know what the results were as soon
    as I can run it.

    I guess I should attempt it with the existing *.xem3 images?

    Thanks again.

    - Juan

  • Hello Marcus,

    Managed to take it out for a spin after all but it didn't give us any different results.

    I was hoping that your version had some extra (or different) pin-muxing or configuration in

    it that would have done the trick compared to what came with the EZSDK but it seems

    like it doesn't. I compared the console traces from your version and the EZSDK one and

    they looked the same. But thank you just the same. One never knows exactly what

    will do the trick so it helps to keep an open mind.

     

    Any other thoughts or insights?

    - Juan