Other Parts Discussed in Thread: TMS320C6713B
Now , i attach vecs_timer1.asm:
******************************************************
* Copyright (C) 2003 Texas Instruments Incorporated
* All Rights Reserved
*
*
*---------vecs_timer1.asm---------
*
* Assembly file to set up interrupt service table (IST)
*
*------------------------------------------------------------------------------
* Global symbols defined here and exported out of this file
*------------------------------------------------------------------------------
.global _vectors
.global _c_int00
.global _vector1
.global _vector2
.global _vector3
.global _vector4
.global _vector5
.global _vector6
.global _vector7
.global _vector8
.global _vector9
.global _vector10
.global _vector11
.global _vector12
.global _vector13
.global _c_int14 ; Hookup the c_int14 ISR in main()
.global _vector15
*------------------------------------------------------------------------------
* Global symbols referenced in this file but defined somewhere else.
* Remember that your interrupt service routines need to be referenced here.
*------------------------------------------------------------------------------
.ref _c_int00
*------------------------------------------------------------------------------
* This is a macro that instantiates one entry in the interrupt service table.
*------------------------------------------------------------------------------
VEC_ENTRY .macro addr
STW B0,*--B15
MVKL addr,B0
MVKH addr,B0
B B0
LDW *B15++,B0
NOP 2
NOP
NOP
.endm
*------------------------------------------------------------------------------
* This is a dummy interrupt service routine used to initialize the IST.
*------------------------------------------------------------------------------
_vec_dummy:
B B3
NOP 5
*------------------------------------------------------------------------------
* This is the actual interrupt service table (IST). It is properly aligned and
* is located in the subsection .text:vecs. This means if you don't explicitly
* specify this section in your linker command file, it will default and link
* into the .text section. Remember to set the ISTP register to point to this
* table.
*------------------------------------------------------------------------------
.sect ".text:vecs"
.align 1024
_vectors:
_vector0: VEC_ENTRY _c_int00 ;RESET
_vector1: VEC_ENTRY _vec_dummy ;NMI
_vector2: VEC_ENTRY _vec_dummy ;RSVD
_vector3: VEC_ENTRY _vec_dummy
_vector4: VEC_ENTRY _vec_dummy
_vector5: VEC_ENTRY _vec_dummy
_vector6: VEC_ENTRY _vec_dummy
_vector7: VEC_ENTRY _vec_dummy
_vector8: VEC_ENTRY _vec_dummy
_vector9: VEC_ENTRY _vec_dummy
_vector10: VEC_ENTRY _vec_dummy
_vector11: VEC_ENTRY _vec_dummy
_vector12: VEC_ENTRY _vec_dummy
_vector13: VEC_ENTRY _vec_dummy
_vector14: VEC_ENTRY _c_int14 ; Hookup the c_int14 ISR in main()
_vector15: VEC_ENTRY _vec_dummy
*------------------------------------------------------------------------------
1 Hi,I don't understand the programme in vecs_timer1.asm file as follows.
******************
VEC_ENTRY .macro addr
STW B0,*--B15
MVKL addr,B0
MVKH addr,B0
B B0
LDW *B15++,B0
NOP 2
NOP
NOP
.endm
*********************
2 What's the functions about B0 and B15?
When isr return,are there must 5 instructions followed that are LDW *B15++,B0 NOW 2 NOP NOP?
Is there must return instruction in the end of isr (c programme)?
3 I think we set address of interrupt programme in the ist and there are eight 32-bit instructions in each fetch package.In the macro of VEC_ENTRY,there are eight instructions.What's the meaning of B B3?
I think each interrupt vector in ist locate on the fetch package boundary,so there are 20h byte offset between each interrupt vector(address of isr).Is that right?
*------------------------------------------------------------------------------
* This is a dummy interrupt service routine used to initialize the IST.
*------------------------------------------------------------------------------
_vec_dummy:
B B3
NOP 5
*------------------------------------------------------------------------------
4 And in time1.c programme,i don't understand the programme set IRQ as follows:
extern far void vectors();
IRQ_setVecs(vectors);
I want to know the address of vectors() and what's the value about ISTP that is the address of IST.
5 Now i use tms320c6713b and I think DSP/BIOS is os on dsp, can i do my work without dsp/bios? What's the difference between DSP/BIOS and no DSP/BIOS project?