now i want use this bus only to download reltek9068 firmware on mcu1_0, and i find the enet driver use mdio "tda4-s2/rtos-sdk/pdk_j721s2/packages/ti/drv/enet" .how can i call mdio driver? the sdk is 8.6 version.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
now i want use this bus only to download reltek9068 firmware on mcu1_0, and i find the enet driver use mdio "tda4-s2/rtos-sdk/pdk_j721s2/packages/ti/drv/enet" .how can i call mdio driver? the sdk is 8.6 version.
Hi,
now i want use this bus only to download reltek9068 firmware on mcu1_0
You mean, want to use MDIO via MCU1_0? If so, we have "enet_lwip_example" application which runs on MCU1_0 with CPSW2G on MCU1_0 in PDK.
Please refer to PDK User Guide for more details. Build the application for MCU1_0/MCU2_1 to use MCU domain CPSW2G.
Best Regards,
Sudheer