This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

when shows"transitioned to executing state",there's nothing on my TV,why?



this is the log;

 

Wait for VM3 to to create the server first

 Entering : OMX_HDVPSS_MicroChain_Test 

#### Initialize the Application Context

#### before OMX_Init() 

#### after OMX_Init() 

You connect the CCS now: Press any key to continue..

 

 Encode: got the component handle

 

 Encode: before setting all Params

 

 Encode: got the component handle

 

 Encode: before setting all Params

 

 Encode: got the component handle

 

 Encode: before setting all Params

 

 Encode: got the component handle

 

 Encode: before setting all Params

VFPC_DEI:0VFPC_SC:0 CTRLTVP Component Transitioned to Idle state 

 VFCC Component Transitioned to Idle state 

 VFPCDEI_0 Component Transitioned to Idle state 

 VENC_0 Component Transitioned to Idle state 

 VENC_1 Component Transitioned to Idle state 

 VENC_2 Component Transitioned to Idle state 

 VENC_3 Component Transitioned to Idle state 

 VDEC_0 Component Transitioned to Idle state 

 VDEC_1 Component Transitioned to Idle state 

 VDEC_2 Component Transitioned to Idle state 

 VDEC_3 Component Transitioned to Idle state 

 VFPCSC Component Transitioned to Idle state 

 CTRLDC_0 Component Transitioned to Idle state 

 VFDC_0 Component Transitioned to Idle state 

 CTRLDC_0 Component Transitioned to Executing state 

 VFDC_0 Component Transitioned to Executing state 

 VFPCSC Component Transitioned to Executing state 

 VDEC_0 Component Transitioned to Executing state 

 VDEC_1 Component Transitioned to Executing state 

 VDEC_2 Component Transitioned to Executing state 

 VDEC_3 Component Transitioned to Executing state 

 VENC_0 Component Transitioned to Executing state 

 VENC_1 Component Transitioned to Executing state 

 VENC_2 Component Transitioned to Executing state 

 VENC_3 Component Transitioned to Executing state 

 VFPCDEI_0 Component Transitioned to Executing state 

 VFCC Component Transitioned to Executing state 

 CTRLTVP Component Transitioned to Executing state 

 

and it stops ,the TV shows  nothing..

what's it suppused to be?

  • there's sth wrong with the connection of TV and splitter. the log is right ,hope it be the reference of VS demo of the 814X

  • "CTRLTVP Component Transitioned to Executing state" is the last thing it says when it's working correctly.

    If you connect some composite video to one or more of the four rightmost yellow RCA jacks on the daugterboard (i.e. the four that are closest to the HDMI connector), then you should see video coming out of the HDMI connector on the daugterboard. Connect the video before starting the demo, not after.