This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: Superspeed USB typo/contradiction

Part Number: AM623


Believe we have a Superspeed USB typo/contradiction between p. 21 and p. 9108 of the TRM https://www.ti.com/lit/pdf/spruiv7  ?

On p, 21

1.4.13 Universal Serial Bus (USB) Subsystem
Instantiated in MAIN domain: Two instances of the Universal Serial Bus (USB) subsystem with integrated
USB2.0 PHY modulehas the following main features:
• Dual-Role Device (DRD) capability
• Support of Peripheral (aka Device) mode at Super Speed (SS at 5 Gbps), High Speed (HS at 480 Mbps), and
Full Speed (FS at 12 Mbps)
• Support of Host mode at Super Speed (SS at 5 Gbps), High Speed (HS at 480 Mbps), Full Speed (FS at 12
Mbps), and Low Speed (LS at 1.5 Mbps

On p. 9108 , I see the opposite clarification for AM62:

>> SuperSpeed (5.0 Gb/s) operation is not supported in either operational mode.

 Please advise?

  • Hello Joe G.

    Thank you for the query.

    Please refer datasheet for the USBSS capabilities and thank you for pointing the discrepancy.

    I will file an internal request to have this updated.

    8.5.21 Universal Serial Bus Subsystem (USBSS)
    USB (Universal Serial Bus) provides a low-cost connectivity solution for numerous consumer portable devices by
    implementing a mechanism for data transfer between USB devices.
    The device instantiates two independent instances of a third-party USB subsystem (USB2SS) operating at up
    to USB2.0 speeds (480Mb/s), either of which can be independently configured to act as a USB Host or a USB
    Device.
    For more information, see Universal Serial Bus Subsystem section in Peripherals chapter in the device TRM.

    Regards,

    Sreenivasa