This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm9000 dm9000.0: read wrong id 0x2b2a2928

Other Parts Discussed in Thread: AM3715

Hello All,

I am working on AM3715 based design (Android Froyo 2.2). Trying to get dm9000 LAN driver working.

I have done all the necessary HW settings for clocks, gpio's etc and verified with the scope.

My software settings in board-omap3evm.c are:

-------------------------------------------------------------------

#define OMAP3EVM_ETHR_START    0x2C000000
#define OMAP3EVM_ETHR_GPIO_IRQ    56
#define OMAP3EVM_DM9000_CS    3

static struct resource dm9k_resource[] = {
    [0] = {
        .start = OMAP3EVM_ETHR_START,
        .end   = (OMAP3EVM_ETHR_START + 3),
        .flags = IORESOURCE_MEM,
    },
    [1] = {
        .start = OMAP3EVM_ETHR_START + 0x8,
        .end   = OMAP3EVM_ETHR_START + 0x8 + 3,
        .flags = IORESOURCE_MEM,
    },
    [2] = {
        .start = OMAP_GPIO_IRQ(OMAP3EVM_ETHR_GPIO_IRQ),
        .end   = OMAP_GPIO_IRQ(OMAP3EVM_ETHR_GPIO_IRQ),
        .flags = (IORESOURCE_IRQ | IRQF_TRIGGER_HIGH),
    },
};

static struct dm9000_plat_data dm9k_platdata = {
    .flags        = DM9000_PLATF_16BITONLY,
};

static struct platform_device device_dm9k = {
    .name        = "dm9000",
    .id        = 0,
    .num_resources    = ARRAY_SIZE(dm9k_resource),
    .resource    = dm9k_resource,
    .dev        = {
        .platform_data = &dm9k_platdata,
    }
};

-----------------------------------------------------------------------

* On EVM the SMSC911x module was connected to GPMC_NCS5, but in our design we are using GPMC_NCS3.

With these settings I am getting following error at the time of boot:

dm9000 Ethernet Driver, V1.31
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: read wrong id 0x2b2a2928
dm9000 dm9000.0: wrong id: 0x2b2a2928
dm9000 dm9000.0: not found (-19).
-------------------------------------------------------------------------

* Is it because I am not setting correct ethernet start address (As we are using CS3)? If yes how could I determine the address?

* Am I missing any settings?

 

Thanks,

-Ninad.