This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Mixed light source scene white light blue

Part Number: TDA4VM

Hi TI Experts,

We have a problem with blue white light in a scene with mixed light sources,which is based on  TI SDK 7.03、J721e_evm and DCC tool v2.5. Our image sensor is OX03C10.

The problem scene has yellow light and white light,As shown in the video, the color of the white light source is normal when it is close to the white light source. When it is far away from the white light source, the white light source is bluer, and the whole picture is bluer.

As can be seen from the log, Bgain increases when moving away from the white light source

Please help us to sovle these cases
Best Regards