Part Number: TDA4VM-Q1
Other Parts Discussed in Thread: TDA4VM
Hello TI Team,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM-Q1
Other Parts Discussed in Thread: TDA4VM
Hello TI Team,
Hi,
xSPI boot mode is supported on J721S2 device, so if you have standard flash supporting this boot mode with SFDP table populated in it, it should work.
Regarding details on this flash, i would request Karan Saxena to help.
Regards,
Brijesh
Hi Juanli Zhang
This device can be supported on J721S2 device.
S28HS512TGABHM01 is there on the J721S2 EVM which is similar to the one you have i.e. S28HS01GTFPBHM03.
The xSPI boot mode on J721E is only supported starting w/ PG 1.1 devices. But if there is limit on J72S2? I didn't find SR1.1 devices in TDA4ECO's DM。
The J721S2 doesn't have a PG 1.1 but the PG 1.0 (or SR 1.0) for J721S2 can support xSPI boot mode.
Regards
Karan