Part Number: TMS320C6678
Hi,TI
I am using bios_mcsdk_02_01_02_06 and ndk 2.21.2.43 on 6678 board.
I want to test the 6678 multicast function. The ndk and socket codes have verified that the multicast function is normal on the 665x platform.
There are similar issues on the forum.
here is my questions:
1. At present, 6678 does not support multicast mode, but 665x platform supports multicast mode; the difference between the two is that 6678 has more PAs, and PA intercepts multicast packets?
2. How can I step by step to troubleshoot the issue? The current phenomenon that can be seen is that recvncfrom has not received data. I hope to check the current status of PA through the register, or which step intercepted the packet message.
3. The chip manual or PDK doc has too little information about PA, can you provide more information links to debug this problem?
4. I refer to the PAUnitTest program and call Pa_configExceptionRoute to enable multicast, but the effect has not improved. The following is my modified code. Please help me to see if there is any error
/*
* nimu_eth.c
*
* Copyright (C) 2011 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/**
* @file nimu_eth_c667x.c
*
* @brief
* Ethernet Packet Driver rewritten using the NIMU Packet
* Architecture guidelines.
*
* Note: The NDK nimu driver interface is built based on the examples from the
* PDK. Please refer to PDK examples
* (<pdk_install_dir>\packages\ti\drv\pa\example\emacExample) directory to get
* the knowledge on the QMSS, CPPI, PA LLD configurations/programs.
*
*/
#include <ti/csl/csl_chipAux.h>
#include <ti/csl/csl_cpsgmiiAux.h>
#include <ti/csl/cslr_cpsgmii.h>
#include <ti/csl/csl_bootcfgAux.h>
#include <ti/transport/ndk/nimu/nimu_eth.h>
#include <ti/sysbios/family/c66/Cache.h>
#include "system/platform.h"
#include "system/resource_mgr.h"
#include "nimu_internal.h"
/* The following code and define is used for code timing measurements of the Tx and Rx routines */
#ifdef TIMING
#include <ti/csl/csl_tsc.h>
#define MAX_TIMING_PACKETS 1000
#endif
#define MAX_CORES 8
uint32_t coreKey [MAX_CORES];
/**
* @brief
* NIMUDeviceTable
*
* @details
* This is the NIMU Device Table for the Platform.
* This should be defined for each platform. Since the current platform
* has a single network Interface; this has been defined here. If the
* platform supports more than one network interface this should be
* defined to have a list of "initialization" functions for each of the
* interfaces.
*/
NIMU_DEVICE_TABLE_ENTRY NIMUDeviceTable[] =
{
/**
* @brief EmacInit for the platform
*/
EmacInit,
EmacInit,
NULL
};
/**
* @b EmacStart
* @n
* The function is used to initialize and start the EMAC
* controller and device.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
static int EmacStart
(
NETIF_DEVICE* ptr_net_device
)
{
EMAC_DATA* ptr_pvt_data;
paMacAddr_t broadcast_mac_addr = { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};
paEthInfo_t ethInfo = { { 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 }, /* Src mac = dont care */
{ 0x10, 0x11, 0x12, 0x13, 0x14, 0x15 }, /* Default Dest mac */
0, /* vlan = dont care */
0, /* ignore ether type */
0 /* MPLS tag = don't care */
};
paRouteInfo_t routeInfo = { pa_DEST_HOST, /* Route a match to the host */
0, /* Flow ID 0 */
0, /* Destination queue */
-1, /* Multi route disabled */
0xaaaaaaaa, /* SwInfo 0 */
0, /* SwInfo 1 is dont care */
0, /* customType = pa_CUSTOM_TYPE_NONE */ \
0, /* customIndex: not used */ \
0, /* pkyType: for SRIO only */ \
NULL /* No commands */
};
/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/* Set inport to correspond to appropriate EMAC port */
if (ptr_pvt_data->pdi.PhysIdx == 0) {
ethInfo.inport = pa_EMAC_PORT_0; //AMC SGMII0
} else {
ethInfo.inport = pa_EMAC_PORT_1; //PHY SGMII1
}
/* Setup Tx */
if (Setup_Tx (ptr_net_device) != 0)
{
printf ("Tx setup failed \n");
return -1;
}
/* Setup Rx */
if (Setup_Rx (ptr_net_device) != 0)
{
printf ("Rx setup failed \n");
return -1;
}
if (Add_ExceptionRoute (ðInfo, &routeInfo) != 0)
{
printf ("Add_ExceptionRoute failed \n");
return -1;
}
memcpy (ðInfo.dst[0], ptr_pvt_data->pdi.bMacAddr, sizeof(paMacAddr_t));
/* Set up the MAC Address LUT*/
if (Add_MACAddress (ðInfo, &routeInfo) != 0)
{
printf ("Add_MACAddress failed \n");
return -1;
}
memcpy (ðInfo.dst[0], broadcast_mac_addr, sizeof(paMacAddr_t));
/* Set up the MAC Address LUT for Broadcast */
if (Add_MACAddress (ðInfo, &routeInfo) != 0)
{
printf ("Add_MACAddress failed \n");
return -1;
}
/* Verify the Tx and Rx Initializations */
if (Verify_Init (ptr_net_device) != 0)
{
printf ("Warning:Queue handler Verification failed \n");
}
/* Copy the MAC Address into the network interface object here. */
mmCopy(&ptr_net_device->mac_address[0], &ptr_pvt_data->pdi.bMacAddr[0], 6);
/* Set the 'initial' Receive Filter */
ptr_pvt_data->pdi.Filter = ETH_PKTFLT_MULTICAST;
ptr_pvt_data->pdi.TxFree = 1;
return 0;
}
/**
* @b EmacStop
* @n
* The function is used to de-initialize and stop the EMAC
* controller and device.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
static int
EmacStop
(
NETIF_DEVICE* ptr_net_device
)
{
EMAC_DATA* ptr_pvt_data;
uint16_t count, i;
Cppi_Desc* pCppiDesc;
uint8_t* bufaddr;
uint32_t bufLen;
/* Disable event, interrupt */
EventCombiner_disableEvent(PLATFORM_ETH_EVENTID);
Hwi_disableInterrupt(PLATFORM_ETH_INTERRUPT);
/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
Osal_nimuFree((Ptr)ptr_pvt_data, platform_roundup(sizeof(EMAC_DATA), PLATFORM_CACHE_LINE_SIZE));
count = Qmss_getQueueEntryCount(gRxQHnd[ptr_pvt_data->pdi.PhysIdx]);
/* Free the packet data buffer associated with the Rx Descriptor */
for (i=0; i < count; i++) {
/* Need to free up the PBM handle */
/* free the PBM packet */
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((QMSS_QPOP (gRxQHnd[ptr_pvt_data->pdi.PhysIdx], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) != NULL)
{
return -1;
}
/* Get the Address and Length for Free */
Cppi_getOriginalBufInfo(Cppi_DescType_HOST, pCppiDesc, &bufaddr, &bufLen);
Osal_nimuFree((Ptr)bufaddr, bufLen);
}
count = Qmss_getQueueEntryCount(gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]);
/* Free the packet data buffer associated with the Rx Descriptor */
for (i=0; i < count; i++) {
/* Need to free up the PBM handle */
/* free the PBM packet */
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((QMSS_QPOP (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) != NULL)
{
return -1;
}
/* Get the Address and Length for Free */
Cppi_getOriginalBufInfo(Cppi_DescType_HOST, pCppiDesc, &bufaddr, &bufLen);
Osal_nimuFree ((Ptr)bufaddr, bufLen);
}
/* tear down queues and dmas */
res_mgr_stop_qmss();
Qmss_queueClose (gPaCfgCmdRespQHnd);
Qmss_queueClose (gTxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]);
Qmss_queueClose (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]);
Qmss_queueClose (gRxQHnd[ptr_pvt_data->pdi.PhysIdx]);
Qmss_queueClose (gTxReturnQHnd[ptr_pvt_data->pdi.PhysIdx]);
for (i = 0; i < NUM_PA_TX_QUEUES; i++)
Qmss_queueClose (gPaTxQHnd[i]);
res_mgr_stop_cppi(CPPI_CFG_PASS);
/* EMAC Controller has been stopped. */
return 0;
}
#ifndef SIMULATOR_SUPPORT
/**
* @b emac_display_linkstatus
* @n
* This function is called whenever there is a change in link state on
* master core.
*
* @param[in] port_num
* EMAC port number.
* @param[in] link_status
* Status of the link.
*
* @retval
* void
*/
void
emac_display_linkstatus
(
uint32_t port_num,
uint32_t link_status
)
{
/* This string array corresponds to link state as defined in csl_mdio.h */
char *LinkStr[] = { "No Link",
"10Mb/s Half Duplex",
"10Mb/s Full Duplex",
"100Mb/s Half Duplex",
"100Mb/s Full Duplex",
"1000Mb/s Full Duplex" };
printf("Port %d Link Status: %s \n",
port_num, LinkStr[link_status]);
}
#endif
/**
* @b EmacPoll
* @n
* The function is used to poll the EMAC controller to check
* if there has been any activity
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
* @param[in] timer_tick
* Flag to poll the driver.
*
* @retval
* void
*/
static void EmacPoll (NETIF_DEVICE* ptr_net_device, uint timer_tick)
{
return;
}
/*
* Routine to debug transmit descriptors
*/
#define DEBUG_TX_DESC 0
#if DEBUG_TX_DESC
#pragma DATA_SECTION(TxDescArray, ".DbgSection");
Cppi_HostDesc TxDescArray[NUM_TX_DESC];
int TxDescArrayIndex = 0;
int gtotal_pkts_freed = 0;
#pragma DATA_SECTION(DescIndexArray, ".DbgSection");
int32_t DescIndexArray[NIMU_NUM_TX_DESC];
int32_t gDescTest = 0;
printHostDesc (Cppi_HostDesc* pHostDesc)
{
printf (" pHostDesc->buffLen =%ld \n" , pHostDesc->buffLen );
printf (" pHostDesc->buffPtr =%ld \n" , pHostDesc->buffPtr );
printf (" pHostDesc->descInfo =%ld \n" , pHostDesc->descInfo );
printf (" pHostDesc->nextBDPtr =%ld \n" , pHostDesc->nextBDPtr );
printf (" pHostDesc->origBufferLen =%ld \n" , pHostDesc->origBufferLen);
printf (" pHostDesc->origBuffPtr =%ld \n" , pHostDesc->origBuffPtr );
printf (" pHostDesc->packetInfo =%ld \n" , pHostDesc->packetInfo );
printf (" pHostDesc->psData =%ld \n" , pHostDesc->psData );
printf (" pHostDesc->softwareInfo0 =%ld \n" , pHostDesc->softwareInfo0);
printf (" pHostDesc->softwareInfo1 =%ld \n" , pHostDesc->softwareInfo1);
printf (" pHostDesc->softwareInfo2 =%ld \n" , pHostDesc->softwareInfo2);
printf (" pHostDesc->tagInfo =%ld \n" , pHostDesc->tagInfo );
printf (" pHostDesc->timeStamp =%ld \n" , pHostDesc->timeStamp );
}
#endif
/**
* @b EmacSend
* @n
* The function is the interface routine invoked by the NDK stack to
* pass packets to the driver.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
* @param[in] hPkt
* Packet to be sent out on wire.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
#ifdef TIMING
#pragma DATA_SECTION(txisr_time, ".TimingSection");
uint32_t txisr_time[MAX_TIMING_PACKETS];
#pragma DATA_SECTION(txisr_time_idx, ".TimingSection");
uint32_t txisr_time_idx = 0;
#pragma DATA_SECTION(txisr_free_count, ".TimingSection");
uint32_t txisr_free_count[MAX_TIMING_PACKETS];
#endif
static int
EmacSend (NETIF_DEVICE* ptr_net_device, PBM_Handle hPkt)
{
EMAC_DATA* ptr_pvt_data;
Cppi_Desc* pCppiDesc;
uint32_t dataBufferSize, i, count=0;
register uint8_t* buffer;
register uint32_t length;
Cppi_HostDesc* pHostDesc;
uint32_t coreNum;
Ptr key;
#ifdef TIMING
CSL_Uint64 st,et;
#endif
#ifdef TIMING
st = 0;
et = 0;
#endif
#ifdef TIMING_TX
/* record start time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
}
#endif
/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/* Begin Critical Section before accessing shared resources. */
key = Osal_cppiCsEnter();
/* Get the core number. */
coreNum = CSL_chipReadReg(CSL_CHIP_DNUM);
count = Qmss_getQueueEntryCount (gTxReturnQHnd[ptr_pvt_data->pdi.PhysIdx]);
/* Check if we got to free up any PBM handles? */
#ifdef TIMING_FREE
if (txisr_time_idx < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
txisr_free_count[txisr_time_idx] = count;
}
#endif
for (i = 0; i < count; i++) {
PBM_Handle hPkt_to_free;
/* Need to free up the PBM handle */
/* free the PBM packet */
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((QMSS_QPOP (gTxReturnQHnd[ptr_pvt_data->pdi.PhysIdx], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) != NULL)
{
goto error_cond;
}
pHostDesc = (Cppi_HostDesc *)pCppiDesc;
/* Software info is intended to hold the PBM Pkt Handle for buffer management */
hPkt_to_free = (PBM_Handle ) pHostDesc->softwareInfo0;
/* Clear the PBM Handle set in the descriptor */
pHostDesc->softwareInfo0 = NULL;
/* Push descriptor to Tx free queue */
QMSS_QPUSH (gTxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
PBM_free( (PBM_Handle) hPkt_to_free);
}
#ifdef TIMING_FREE
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}
#endif
/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/* Make sure the driver does not transmit packet less than min. as per the
* Ethernet standards. */
if( PBM_getValidLen(hPkt) < 60 )
PBM_setValidLen (hPkt, 64 );
/* We do not do any packet size checks here. If the packet
* is too big to fit in the MTU configured on the peripheral,
* then the driver/CSL layer should catch the error.
*/
if(1)
{
/* Peek into the packet to check out if any
* prioritization is needed.
*
* All raw Ethernet packets are tagged with the EMAC
* channel number onto which they need to be sent out
* in the PktPriority field.
*/
if (((PBM_Pkt *)hPkt)->PktPriority != PRIORITY_UNDEFINED)
{
/* PktPriority contains the EMAC channel number on which
* the packet needs to be txed.
*/
ptr_pvt_data->pdi.PhysIdx = (((PBM_Pkt *)hPkt)->PktPriority);
}
else
{
/* This is just a normal IP packet. Enqueue the packet in the
* Tx queue and send it for transmission.
* We are assuming here that the IP packets are transmitted
* on Channel 0 -> Core 0; Channel 1 --> Core 1; Channel 2 --> Core 2.
* and that the Raw packets can be transmitted on any channel.
*/
ptr_pvt_data->pdi.PhysIdx = ptr_pvt_data->pdi.PhysIdx;
}
/* Pass the packet to the controller if the transmitter is free. */
if(ptr_pvt_data->pdi.TxFree )
{
buffer = PBM_getDataBuffer(hPkt) + PBM_getDataOffset(hPkt);
length = PBM_getValidLen(hPkt);
/* Clean the cache for external/L2 addresses */
if( ((uint32_t)buffer & EMAC_EXTMEM ) ||
((uint32_t)buffer & EMAC_LL2SRAM ) ) {
OEMCacheClean( (void *)buffer, length );
}
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((QMSS_QPOP (gTxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) != NULL) {
// Wait for transmitted packet to return
while ((QMSS_QPOP (gTxReturnQHnd[ptr_pvt_data->pdi.PhysIdx], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) != 0);
pHostDesc = (Cppi_HostDesc *)pCppiDesc;
// free the PBM packet
PBM_free((PBM_Handle)pHostDesc->softwareInfo0);
}
pHostDesc = (Cppi_HostDesc *)pCppiDesc;
pHostDesc->softwareInfo0 = (uint32_t) hPkt;
dataBufferSize = length;
Cppi_setData ( Cppi_DescType_HOST,
(Cppi_Desc *) pCppiDesc,
(uint8_t *) Convert_CoreLocal2GlobalAddr((uint32_t)buffer),
dataBufferSize
);
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, dataBufferSize);
count = Qmss_getQueueEntryCount (gTxReturnQHnd[ptr_pvt_data->pdi.PhysIdx]);
#ifdef PA_LOOPBACK
QMSS_QPUSH (gPaTxQHnd[0], pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);
#else
if (ptr_pvt_data->pdi.PhysIdx == 0) {
gTxPort = pa_EMAC_PORT_0; // AMC SGMII0
} else {
gTxPort = pa_EMAC_PORT_1; // PHY SGMII1
}
Cppi_setPSFlags (Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, gTxPort);
/* Send the packet out the mac. It will loop back to PA if the mac/switch
* have been configured properly
*/
QMSS_QPUSH (gPaTxQHnd[8], pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);
#endif
/* Increment the application transmit counter */
gTxCounter ++;
}
/* Packet has been successfully transmitted. */
/* End Critical Section */
Osal_cppiCsExit (key);
#ifdef TIMING_TX
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}
#endif
return 0;
}
error_cond:
{
/* End Critical Section */
Osal_cppiCsExit (key);
#ifdef TIMING_TX
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}
#endif
return -1;
}
}
/**
* @b Description
* @n
* Call back function provided by application for EMAC driver
* to report a received packet descriptor.
*
* @retval
* None.
*/
static Bool gIsPingListUsed = 0;
#ifdef TIMING
#pragma DATA_SECTION(rxisr_time, ".TimingSection");
uint32_t rxisr_time[MAX_TIMING_PACKETS]; /* hold start time, end time, start time, end time, etc */
#pragma DATA_SECTION(rxisr_time_idx, ".TimingSection");
uint32_t rxisr_time_idx;
#pragma DATA_SECTION(rxisr_pktcount, ".TimingSection");
uint32_t rxisr_pktcount;
#endif
void
EmacRxPktISR
(
NETIF_DEVICE* ptr_net_device
)
{
uint32_t protocol, pktLen;
uint8_t* pBuffer;
Cppi_HostDesc* pHostDesc;
PBM_Handle hPkt;
Cppi_Desc* pCppiDesc;
uint32_t count, i;
uint32_t* ListAddress;
EMAC_DATA* ptr_pvt_data;
PBM_Pkt* rx_pbm_pkt;
void* key;
void* accum_list_ptr;
#ifdef TIMING
CSL_Uint64 st, et;
#endif
#ifdef TIMING
/* record start time */
if (rxisr_pktcount < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
}
#endif
/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/* Disable the interrupt */
coreKey [CSL_chipReadReg (CSL_CHIP_DNUM)] = Hwi_disableInterrupt(ptr_pvt_data->vector_id);
/* Begin Critical Section before accessing shared resources. */
key = Osal_qmssCsEnter ();
gIsPingListUsed = ptr_pvt_data->IsPingListUsed;
if (!gIsPingListUsed){
accum_list_ptr = (void *)&ptr_pvt_data->HiPriAccumList[0];
}
else {
accum_list_ptr = (void *)&ptr_pvt_data->HiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE];
}
/* Invalidate cache if needed --
* if accumulator is in DDR then INV L2.
* if accumulator is in shared RAM (MSMC) invalidate L1
*/
if((uint32_t)(ptr_pvt_data->HiPriAccumList) & EMAC_EXTMEM ){
Cache_inv(accum_list_ptr, sizeof(ptr_pvt_data->HiPriAccumList)/2, Cache_Type_L2, CACHE_WAIT);
}
if((uint32_t)(ptr_pvt_data->HiPriAccumList) & EMAC_MSMCSRAM ){
Cache_inv(accum_list_ptr, sizeof(ptr_pvt_data->HiPriAccumList)/2, Cache_Type_L1D, CACHE_WAIT);
}
i = MAX_HI_PRI_ACCUM_LIST_SIZE - 1 - (RX_INT_THRESHOLD);
ListAddress = (uint32_t* )Convert_CoreLocal2GlobalAddr((uint32_t) &ptr_pvt_data->HiPriAccumList[i]);
/* Process ISR.
*
* Get the number of entries in accumulator list.
* The hardware enqueues data alternatively to Ping/Pong buffer lists in
* the accumulator. Hence, we need to track which list (Ping/Pong)
* we serviced the last time and accordingly process the other one
* this time around.
*/
if (!gIsPingListUsed)
{
/* Serviced Pong list last time. So read off the Ping list now */
count = ListAddress[0];
}
else
{
/* Serviced Pong list last time. So read off the Ping list now */
count = ListAddress[RX_INT_THRESHOLD + 1];
}
/* Nothing to receive, so return... */
if (count == 0) {
/* End Critical Section */
Osal_qmssCsExit (key);
Hwi_restoreInterrupt(ptr_pvt_data->vector_id, coreKey [CSL_chipReadReg (CSL_CHIP_DNUM)]);
/* Clear INTD */
Qmss_ackInterrupt(ptr_pvt_data->acc_channel_num, 1);
Qmss_setEoiVector(Qmss_IntdInterruptType_HIGH, ptr_pvt_data->acc_channel_num);
return ; /* Not enough packets are received */
}
/* Process all the Results received
*
* Skip the first entry in the list that contains the
* entry count and proceed processing results.
*/
for (i = 1; i <= count; i ++)
{
gRxCounter ++;
/* Get the result descriptor.
*
* The hardware enqueues data alternatively to Ping/Pong buffer lists in
* the accumulator. Hence, we need to track which list (Ping/Pong)
* we serviced the last time and accordingly process the other one
* this time around.
*/
if (!gIsPingListUsed)
{
/* Serviced Pong list last time. So read off the Ping list now */
pCppiDesc = (Cppi_Desc *) ListAddress [i];
}
else
{
/* Serviced Ping list last time. So read off the Pong list now
*
* Skip over Ping list length to arrive at Pong list start.
*/
pCppiDesc = (Cppi_Desc *) ListAddress [i + RX_INT_THRESHOLD + 1];
}
/* Descriptor size appended to the address in the last 4 bits.
*
* To get the true descriptor size, always mask off the last
* 4 bits of the address.
*/
pCppiDesc = (Ptr) ((uint32_t) pCppiDesc & 0xFFFFFFF0);
pHostDesc = (Cppi_HostDesc *)pCppiDesc;
/* Invalidate cache based on where the memory is */
if((uint32_t)(pHostDesc) & EMAC_EXTMEM ){
Cache_inv((void *) pHostDesc, sizeof(Cppi_HostDesc), Cache_Type_L2, CACHE_WAIT);
}
if ((uint32_t)(pHostDesc) & EMAC_MSMCSRAM ) {
Cache_inv((void *)pHostDesc, sizeof(Cppi_HostDesc), Cache_Type_L1D, CACHE_WAIT);
}
if((uint32_t)(pHostDesc->buffPtr) & EMAC_EXTMEM ){
Cache_inv((void *) pHostDesc->buffPtr, pHostDesc->buffLen, Cache_Type_L2, CACHE_WAIT);
}
if ((uint32_t)(pHostDesc->buffPtr) & EMAC_MSMCSRAM ) {
Cache_inv((void *)pHostDesc->buffPtr, pHostDesc->buffLen, Cache_Type_L1D, CACHE_WAIT);
}
/*
* We should not see packets too large but check anyways ...
* Note that we are subtracting off the FCS the switch added to the frame.
* If its too large then return it to the free queue.
*/
if ((pHostDesc->buffLen-4) > (ptr_net_device->mtu + ETHHDR_SIZE)) {
/* lets try the next one... we should record this as a too large.... */
gRxDropCounter++;
pHostDesc->buffLen = pHostDesc->origBufferLen;
QMSS_QPUSH (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
continue;
}
/* Allocate the PBM packet for the Max MTU size*/
if (NULL == (hPkt = PBM_alloc(1514))) {
/* could not get a free NDK packet, maybe the next time around we can... */
gRxDropCounter++;
pHostDesc->buffLen = pHostDesc->origBufferLen;
QMSS_QPUSH (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
continue;
}
rx_pbm_pkt = (PBM_Pkt *) hPkt;
PBM_setDataOffset((PBM_Handle) hPkt, 0);
/* removing the FCS length the EMAC switch adds here */
pktLen = (pHostDesc->buffLen-4);
/* Set to minimum packet size */
if (pktLen < 60) {
pktLen = 64;
}
PBM_setValidLen((PBM_Handle) hPkt, pktLen);
/* Handle raw frames separately, i.e. check the
* Ethernet Protocol type in this packet and see
* if its a well known ether type. If so, this is normal
* IP stream, enqueue this is in usual Rx queue and let the
* stack know that a packet has arrived for it. However, if
* the Ethernet type in the packet is not a well known one,
* this could be a custom raw Ethernet packet, enqueue it
* separately in the Raw Rx queue and notify stack. The Raw
* Ethernet packets when being handed over are given
* preferential treatment and are serviced before the normal
* IP traffic. Hence the 2 queues.
*/
pBuffer = (uint8_t* )Convert_CoreLocal2GlobalAddr((uint32_t) pHostDesc->buffPtr);
/* Extract the Ethernet type from the packet. */
protocol = ( pBuffer[12] << 8) | pBuffer[13] ;
protocol = (protocol & 0xFFFFu);
PBM_setIFRx((PBM_Handle) hPkt, (HANDLE) protocol );
/* Copy the data buffer received to the allocated PBM packet */
mmCopy((uint8_t* )rx_pbm_pkt->pDataBuffer, (uint8_t* )pBuffer, pktLen) ;
/* Is it a standard ethernet type? */
if (protocol != ETHERTYPE_IP && protocol != ETHERTYPE_IPv6 && protocol != ETHERTYPE_VLAN
&& protocol != ETHERTYPE_PPPOECTL && protocol != ETHERTYPE_PPPOEDATA )
{
/* This is a raw packet, enqueue in Raw Rx Queue */
PBMQ_enq( &ptr_pvt_data->pdi.PBMQ_rawrx, (PBM_Handle) hPkt);
}
else
{ /* This is a normal IP packet. Enqueue in Rx Queue */
PBMQ_enq( &ptr_pvt_data->pdi.PBMQ_rx, (PBM_Handle) hPkt );
}
/* Free the packet back to the Rx FDQ */
pHostDesc->buffLen = pHostDesc->origBufferLen;
QMSS_QPUSH (gRxFreeQHnd[0], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
}
ListAddress = (uint32_t *) Convert_CoreLocal2GlobalAddr((uint32_t) &ptr_pvt_data->HiPriAccumList[0]);
/* Clear the accumulator list and save whether we used Ping/Pong
* list information for next time around.
*/
if (!gIsPingListUsed)
{
/* Just processed Ping list */
gIsPingListUsed = 1;
i = sizeof (ptr_pvt_data->HiPriAccumList)/2;
/* Clear the accumulator list after processing */
memset ((Void *) &ptr_pvt_data->HiPriAccumList[0], 0, i);
if(
((uint32_t)(&ptr_pvt_data->HiPriAccumList[0]) & EMAC_EXTMEM ) ||
((uint32_t)(&ptr_pvt_data->HiPriAccumList[0]) & EMAC_MSMCSRAM )
)
{
/* This needs to be enabled if gHiPriAccumList is in External Memory or MSMCMEM */
Cache_wb ((void *)&ptr_pvt_data->HiPriAccumList[0], i, Cache_Type_L2, CACHE_WAIT);
}
}
else
{
/* Just processed Pong list */
gIsPingListUsed = 0;
i = sizeof (ptr_pvt_data->HiPriAccumList)/2;
/* Clear the accumulator list after processing */
memset ((Void *) &ptr_pvt_data->HiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE], 0, i);
if(
((uint32_t)(&ptr_pvt_data->HiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE]) & EMAC_EXTMEM ) ||
((uint32_t)(&ptr_pvt_data->HiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE]) & EMAC_MSMCSRAM )
)
{
/* This needs to be enabled if gHiPriAccumList is in External Memory or MSMCMEM */
Cache_wb((void *) &ptr_pvt_data->HiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE], i, Cache_Type_L2, CACHE_WAIT);
}
}
ptr_pvt_data->IsPingListUsed = gIsPingListUsed;
/* Notify NDK stack of pending Rx Ethernet packet */
STKEVENT_signal( ptr_pvt_data->pdi.hEvent, STKEVENT_ETHERNET, 1 );
/* End Critical Section */
Osal_qmssCsExit (key);
Hwi_restoreInterrupt(ptr_pvt_data->vector_id, coreKey [CSL_chipReadReg (CSL_CHIP_DNUM)]);
#ifdef TIMING
/* record end time */
if (rxisr_pktcount < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
rxisr_time[rxisr_time_idx++] = (uint32_t) (et-st);
rxisr_pktcount += count;
}
#endif
/* Clear INTD */
Qmss_ackInterrupt(ptr_pvt_data->acc_channel_num, 1);
Qmss_setEoiVector(Qmss_IntdInterruptType_HIGH, ptr_pvt_data->acc_channel_num);
return;
}
/**
* @b EmacPktService
* @n
* The function is called by the NDK core stack to receive any packets
* from the driver.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
*
* @retval
* void
*/
static void EmacPktService (NETIF_DEVICE* ptr_net_device)
{
EMAC_DATA* ptr_pvt_data;
PBM_Handle hPacket;
/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/* Give all queued Raw packets first to the Ether module */
while (PBMQ_count(&ptr_pvt_data->pdi.PBMQ_rawrx))
{
/* Dequeue a packet from the driver's Raw receive queue. */
hPacket = PBMQ_deq(&ptr_pvt_data->pdi.PBMQ_rawrx);
/* Prepare the packet so that it can be passed up the networking stack.
* If this 'step' is not done the fields in the packet are not correct
* and the packet will eventually be dropped. */
PBM_setIFRx (hPacket, ptr_net_device);
/* Pass the packet to the NDK Core stack. */
NIMUReceivePacket(hPacket);
}
/* Give all queued IP packets to the Ether module */
while (PBMQ_count(&ptr_pvt_data->pdi.PBMQ_rx))
{
/* Dequeue a packet from the driver receive queue. */
hPacket = PBMQ_deq(&ptr_pvt_data->pdi.PBMQ_rx);
/* Prepare the packet so that it can be passed up the networking stack.
* If this 'step' is not done the fields in the packet are not correct
* and the packet will eventually be dropped. */
PBM_setIFRx (hPacket, ptr_net_device);
/* Pass the packet to the NDK Core stack. */
NIMUReceivePacket(hPacket);
}
/* Work has been completed; the receive queue is empty... */
return;
}
/**
* @b Emacioctl
* @n
* The function is called by the NDK core stack to configure the
* driver
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
* @param[in] cmd
* Ioctl command.
* @param[in] pBuf
* Mac address to be added or deleted.
* @param[in] size
* Size of Mac Address.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
static int Emacioctl (NETIF_DEVICE* ptr_net_device, uint cmd, void* pBuf, uint size)
{
return 0;
}
/**
* @b EmacInit
* @n
* The function is used to initialize and register the EMAC
* with the Network Interface Management Unit (NIMU)
*
* @param[in] hEvent
* Stack Event Handle.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
static int EmacInit (STKEVENT_Handle hEvent)
{
EMACInit_Core(hEvent);
return 0;
}
static int EMACInit_Core (STKEVENT_Handle hEvent)
{
NETIF_DEVICE* ptr_device;
EMAC_DATA* ptr_pvt_data;
char names[6][5]={"eth0","eth1","eth2","eth3","eth4","eth5"};
uint32_t coreNum, i;
PLATFORM_EMAC_EXT_info emac_info;
/* number of emac interface instantiated */
static int numEmacInterfaces = 0;
/* Get the core number. */
coreNum = CSL_chipReadReg(CSL_CHIP_DNUM);
/* Allocate memory for the private data */
ptr_pvt_data = Osal_nimuMalloc (platform_roundup(sizeof(EMAC_DATA), PLATFORM_CACHE_LINE_SIZE), PLATFORM_CACHE_LINE_SIZE);
if (ptr_pvt_data == NULL)
{
printf ("Error: Unable to allocate private memory data\n");
return -1;
}
/* Initialize the allocated memory block. */
mmZeroInit (ptr_pvt_data, sizeof(EMAC_DATA));
/* Initialize the RX Queue */
PBMQ_init(&ptr_pvt_data->pdi.PBMQ_rx);
PBMQ_init(&ptr_pvt_data->pdi.PBMQ_rawrx);
/* Initialize the private data */
mmZeroInit(&ptr_pvt_data->pdi, sizeof(PDINFO));
/* Set physical index
* Essentially corresponds PhysIdx to interface. First interface EMACInit_Core is called
* gets PhysIdx to 0, second interface to call gets PhysIdx of one
* Note: Assumes PHY interface is initialized first, AMC second
*/
ptr_pvt_data->pdi.PhysIdx = numEmacInterfaces;
ptr_pvt_data->pdi.hEvent = hEvent;
/* MCast List is EMPTY */
ptr_pvt_data->pdi.MCastCnt = 0;
if (ptr_pvt_data->pdi.PhysIdx == 0) {
ptr_pvt_data->event_id = PLATFORM_AMC_EVENTID;
ptr_pvt_data->acc_channel_num = PA_ACC_CHANNEL_NUM_SEC_INTERFACE;
ptr_pvt_data->vector_id = PLATFORM_AMC_INTERRUPT;
ptr_pvt_data->HiPriAccumList = (uint32_t*)gHiPriAccumList_sec;
} else {
ptr_pvt_data->event_id = PLATFORM_ETH_EVENTID;
ptr_pvt_data->acc_channel_num = PA_ACC_CHANNEL_NUM;
ptr_pvt_data->vector_id = PLATFORM_ETH_INTERRUPT;
ptr_pvt_data->HiPriAccumList = (uint32_t*)gHiPriAccumList;
}
ptr_pvt_data->IsPingListUsed = 0;
#ifndef SIMULATOR_SUPPORT
for (i = 0; i < PLATFORM_MAX_EMAC_PORT_NUM; i++)
{
platform_get_emac_info (i, &emac_info);
if (emac_info.mode == PLATFORM_EMAC_PORT_MODE_PHY && ptr_pvt_data->pdi.PhysIdx == 1)
{
printf("\tPHY = SGMII port %d\n", i);
break;
}
if (emac_info.mode == PLATFORM_EMAC_PORT_MODE_AMC && ptr_pvt_data->pdi.PhysIdx == 0)
{
printf("\tAMC = SGMII port %d\n", i);
/* Increment last bit of MAC address to provide second interface with unique MAC */
emac_info.mac_address[5]++;
break;
}
}
if (i < PLATFORM_MAX_EMAC_PORT_NUM)
{
gTxPort = emac_info.port_num;
memcpy(ptr_pvt_data->pdi.bMacAddr, emac_info.mac_address, 6);
}
else
{
printf ("Error: Unable to find a TX EMAC port\n");
return -1;
}
#else
{
gTxPort = 1;
platform_get_emac_info (1, &emac_info);
memcpy(ptr_pvt_data->pdi.bMacAddr, emac_info.mac_address, 6);
}
#endif
/* Init Logical Device */
/* ptr_pvt_data->pdi.hEther = hEther; */
/* Allocate memory for the EMAC. */
/* ptr_device needs to be allocated via mmAlloc since NDK frees it during shutdown */
ptr_device = mmAlloc(sizeof(NETIF_DEVICE));
if (ptr_device == NULL)
{
printf ("Error: Unable to allocate memory for the EMAC\n");
return -1;
}
/* Initialize the allocated memory block. */
mmZeroInit (ptr_device, sizeof(NETIF_DEVICE));
/* Populate the Network Interface Object. */
strcpy (ptr_device->name, names[numEmacInterfaces]);
ptr_device->mtu = ETH_MAX_PAYLOAD - ETHHDR_SIZE;
ptr_device->pvt_data = (void *)ptr_pvt_data;
/* Populate the Driver Interface Functions. */
ptr_device->start = EmacStart;
ptr_device->stop = EmacStop;
ptr_device->poll = EmacPoll;
ptr_device->send = EmacSend;
ptr_device->pkt_service = EmacPktService;
ptr_device->ioctl = Emacioctl;
ptr_device->add_header = NIMUAddEthernetHeader;
/*
* PASS and Cpsw only need to be initialized once, so do it when first interface calls
* this init function
*/
if (ptr_pvt_data->pdi.PhysIdx == 0) {
/* Init PA LLD */
if (Init_PASS () != 0)
{
printf ("PASS init failed \n");
return -1;
}
else
{
printf ("PASS successfully initialized \n");
}
/* Initialize the CPSW switch */
if (Init_Cpsw ((uint32_t) ptr_device->mtu, ptr_pvt_data->pdi.bMacAddr) != 0)
{
printf ("Ethernet subsystem init failed \n");
return -1;
}
else
{
printf ("Ethernet subsystem successfully initialized \n");
}
}
numEmacInterfaces++;
/* Set NIMU Interface ID */
if (ptr_pvt_data->pdi.PhysIdx == 0) {
ptr_device->index = pa_EMAC_PORT_0; // AMC SGMII0
} else {
ptr_device->index = pa_EMAC_PORT_1; // PHY SGMII1
}
/* Register the device with NIMU */
if (NIMURegister (ptr_device) < 0)
{
printf ("Error: Unable to register the EMAC\n");
return -1;
}
printf ("Registration of the EMAC Successful, waiting for link up ..\n");
return 0;
}
/** ============================================================================
* @n@b Setup_Tx
*
* @b Description
* @n This API sets up all relevant data structures and configuration required
* for sending data to PASS/Ethernet. It sets up a Tx free descriptor queue,
* PASS Tx queues required for send.
*
* @param[in]
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Setup_Tx (NETIF_DEVICE* ptr_net_device)
{
uint8_t isAllocated, i;
Qmss_Queue qRetInfo;
Ptr pCppiDesc;
uint32_t mySWInfo[] = {0x00000000, 0x00000000, 0x00000000};
int index = 0;
EMAC_DATA* ptr_pvt_data;
/* Open all Transmit (Tx) queues.
*
* These queues are used to send data to PA PDSP/CPSW.
*/
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/* Use different gHiPriAccumList depending on interface */
if (ptr_pvt_data->pdi.PhysIdx == 0) {
index = 0;
for (i = 0; i < NUM_PA_TX_QUEUES; i ++)
{
if ((gPaTxQHnd[i] = Qmss_queueOpen (Qmss_QueueType_PASS_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening PA Tx queue \n");
return -1;
}
}
} else {
index = 1;
}
/* Open a Tx Free Descriptor Queue (Tx FDQ).
*
* This queue will be used to hold Tx free decriptors that can be filled
* later with data buffers for transmission onto wire.
*/
if ((gTxFreeQHnd[index] = Qmss_queueOpen (Qmss_QueueType_STARVATION_COUNTER_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening Tx Free descriptor queue \n");
return -1;
}
/* Open a Tx Return Descriptor Queue (Tx Transmit CompletionQ).
*
* This queue will be used to hold Tx completed decriptors that can be filled
* later with data buffers for transmission onto wire.
*/
if ((gTxReturnQHnd[index] = Qmss_queueOpen (Qmss_QueueType_GENERAL_PURPOSE_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening Tx Return descriptor queue \n");
return -1;
}
qRetInfo = Qmss_getQueueNumber (gTxReturnQHnd[index]);
/* Attach some free descriptors to the Tx free queue we just opened. */
for (i = 0; i < NIMU_NUM_TX_DESC; i++)
{
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((QMSS_QPOP (res_mgr_qmss_get_freeq(), QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc )) != NULL)
{
break;
}
/* Setup the Completion queue:
*
* Setup the return policy for this desc to return to the completion q we just
* setup instead of the global free queue.
*/
Cppi_setReturnQueue ((Cppi_DescType) Cppi_DescType_HOST, pCppiDesc, qRetInfo);
/* Software info is inteded to hold the PBM Pkt Handle for buffer management */
mySWInfo[1] = i;
Cppi_setSoftwareInfo (Cppi_DescType_HOST, pCppiDesc, (uint8_t *) mySWInfo);
/* Push descriptor to Tx free queue */
QMSS_QPUSHDESCSIZE (gTxFreeQHnd[index], pCppiDesc, SIZE_HOST_DESC);
}
if (i != NIMU_NUM_TX_DESC)
{
printf ("Error allocating Tx free descriptors \n");
return -1;
}
/* Open a Tx Command Free Descriptor Queue (Tx CMD FDQ).
*
* This queue will be used to hold Tx Command free decriptors
*/
if ((gTxCmdFreeQHnd[index] = Qmss_queueOpen (Qmss_QueueType_STARVATION_COUNTER_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening Tx Cmd Free descriptor queue \n");
return -1;
}
/* Open a Tx Cmd Return Descriptor Queue (Tx Cmd Completion Queue).
*
* This queue will be used to hold Tx command completed decriptors
*/
if ((gTxCmdReturnQHnd[index] = Qmss_queueOpen (Qmss_QueueType_GENERAL_PURPOSE_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening Tx Return descriptor queue \n");
return -1;
}
qRetInfo = Qmss_getQueueNumber (gTxCmdReturnQHnd[index]);
/* Attach some free descriptors to the Tx CMD free queue we just opened. */
for (i = 0; i < NIMU_MAX_NUM_TX_CMD_DESC; i++)
{
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((QMSS_QPOP (res_mgr_qmss_get_freeq(), QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc )) != NULL)
{
break;
}
/* Setup the Completion queue:
*
* Setup the return policy for this desc to return to the completion q we just
* setup instead of the global free queue.
*/
Cppi_setReturnQueue ((Cppi_DescType) Cppi_DescType_HOST, pCppiDesc, qRetInfo);
/* Push descriptor to Tx free queue */
QMSS_QPUSHDESCSIZE (gTxCmdFreeQHnd[index], pCppiDesc, SIZE_HOST_DESC);
}
if (i != NIMU_MAX_NUM_TX_CMD_DESC)
{
printf ("Error allocating Tx Command free descriptors \n");
return -1;
}
/* All done with Rx configuration. Return success. */
return 0;
}
/** ============================================================================
* @n@b Setup_Rx
*
* @b Description
* @n This API sets up all relevant data structures and configuration required
* for receiving data from PASS/Ethernet. It sets up a Rx free descriptor queue
* with some empty pre-allocated buffers to receive data, and an Rx queue
* to which the Rxed data is streamed for the example application. This API
* also sets up the QM high priority accumulation interrupts required to
* receive data from the Rx queue.
*
* @param[in]
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Setup_Rx (NETIF_DEVICE* ptr_net_device)
{
int32_t result, vectId;
uint8_t isAllocated, accChannelNum, i;
uint16_t numAccEntries, intThreshold, pktLen;
Qmss_Queue rxFreeQInfo, rxQInfo;
Ptr pCppiDesc;
Qmss_AccCmdCfg accCfg;
Cppi_RxFlowCfg rxFlowCfg;
int16_t eventId;
Ptr pDataBuffer;
uint32_t mySWInfo[] = {0x11112222, 0x33334444, 0x55556666};
uint32_t ListAddress;
EMAC_DATA* ptr_pvt_data;
int32_t count;
pktLen = ptr_net_device->mtu + ETHHDR_SIZE + 4; /* ETh Header + 4 bytes of FCS */
pktLen += 128; /* 128Byte gap in order to prevent prefetch buffer problems */
i = MAX_HI_PRI_ACCUM_LIST_SIZE - 1 - (RX_INT_THRESHOLD);
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/* Use different gHiPriAccumList depending on interface */
ListAddress = Convert_CoreLocal2GlobalAddr((uint32_t) &ptr_pvt_data->HiPriAccumList[i]);
/* Open a Receive (Rx) queue.
*
* This queue will be used to hold all the packets received by PASS/CPSW
*
* Open the next available High Priority Accumulation queue for Rx.
*/
if ((gRxQHnd[ptr_pvt_data->pdi.PhysIdx] = Qmss_queueOpen (Qmss_QueueType_HIGH_PRIORITY_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening a High Priority Accumulation Rx queue \n");
return -1;
}
rxQInfo = Qmss_getQueueNumber (gRxQHnd[ptr_pvt_data->pdi.PhysIdx]);
/* Setup high priority accumulation interrupts on the Rx queue.
*
* Let's configure the accumulator with the following settings:
* (1) Interrupt pacing disabled.
* (2) Interrupt on every received packet
*/
intThreshold = RX_INT_THRESHOLD;
numAccEntries = (intThreshold + 1) * 2;
accChannelNum = ptr_pvt_data->acc_channel_num;
/* Initialize the accumulator list memory */
memset ((Void *) ListAddress, 0, numAccEntries * 4);
/* Ensure that the accumulator channel we are programming is not
* in use currently.
*/
result = Qmss_disableAccumulator (Qmss_PdspId_PDSP1, accChannelNum);
if (result != QMSS_ACC_SOK && result != QMSS_ACC_CHANNEL_NOT_ACTIVE)
{
printf ("Error Disabling high priority accumulator for channel : %d error code: %d\n",
accChannelNum, result);
return -1;
}
/* Setup the accumulator settings */
accCfg.channel = accChannelNum;
accCfg.command = Qmss_AccCmd_ENABLE_CHANNEL;
accCfg.queueEnMask = 0;
accCfg.listAddress = ListAddress;
accCfg.queMgrIndex = gRxQHnd[ptr_pvt_data->pdi.PhysIdx];
accCfg.maxPageEntries = (intThreshold + 1); /* Add an extra entry for holding the entry count */
accCfg.timerLoadCount = 5;
accCfg.interruptPacingMode = Qmss_AccPacingMode_LAST_INTERRUPT;
accCfg.listEntrySize = Qmss_AccEntrySize_REG_D;
accCfg.listCountMode = Qmss_AccCountMode_ENTRY_COUNT;
accCfg.multiQueueMode = Qmss_AccQueueMode_SINGLE_QUEUE;
/* Program the accumulator */
if ((result = Qmss_programAccumulator (Qmss_PdspId_PDSP1, &accCfg)) != QMSS_ACC_SOK)
{
printf ("Error Programming high priority accumulator for channel : %d queue : %d error code : %d\n",
accCfg.channel, accCfg.queMgrIndex, result);
return -1;
}
/* Register interrupts for the system event corresponding to the
* accumulator channel we are using.
*/
/* System event n - Accumulator Channel 0 */
eventId = ptr_pvt_data->event_id;
vectId = ptr_pvt_data->vector_id;
printf ("Ethernet eventId : %d and vectId (Interrupt) : %d \n", eventId, vectId);
/* Register our ISR handle for this event */
EventCombiner_dispatchPlug (eventId, (EventCombiner_FuncPtr)EmacRxPktISR, (UArg)ptr_net_device, TRUE);
EventCombiner_enableEvent(eventId);
/* Map the event id to hardware interrupt 7. */
Hwi_eventMap(vectId, eventId >> 5);
/* Enable interrupt */
Hwi_enableInterrupt(vectId);
/* Open a Rx Free Descriptor Queue (Rx FDQ).
*
* This queue will hold all the Rx free descriptors. These descriptors will be
* used by the PASS CPDMA to hold data received via CPSW.
*/
if ((gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx] = Qmss_queueOpen (Qmss_QueueType_STARVATION_COUNTER_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening Rx Free descriptor queue \n");
return -1;
}
rxFreeQInfo = Qmss_getQueueNumber (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]);
/* Attach some free descriptors to the Rx free queue we just opened. */
for (i = 0; i < NIMU_NUM_RX_DESC; i++)
{
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((QMSS_QPOP (res_mgr_qmss_get_freeq(), QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) != NULL)
{
break;
}
pktLen = platform_roundup(pktLen, PLATFORM_CACHE_LINE_SIZE);
if ((pDataBuffer = Osal_nimuMalloc (pktLen, PLATFORM_CACHE_LINE_SIZE)) == NULL)
{
printf ("Error allocating memory for Rx data buffer \n");
break;
}
/* Populate the Rx free descriptor with the buffer we just allocated. */
Cppi_setData (Cppi_DescType_HOST, pCppiDesc, (uint8_t *)Convert_CoreLocal2GlobalAddr((uint32_t)pDataBuffer) + 128, pktLen);
/* Save original buffer information */
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, pCppiDesc, (uint8_t *)Convert_CoreLocal2GlobalAddr((uint32_t)pDataBuffer), pktLen);
/* Setup the Completion queue:
*
* Setup the return policy for this desc to return to the free q we just
* setup instead of the global free queue.
*/
Cppi_setReturnQueue (Cppi_DescType_HOST, pCppiDesc, rxFreeQInfo);
Cppi_setSoftwareInfo (Cppi_DescType_HOST, pCppiDesc, (uint8_t *) mySWInfo);
Cppi_setPacketLen (Cppi_DescType_HOST, pCppiDesc, pktLen);
/* Push descriptor to Rx free queue */
QMSS_QPUSHDESCSIZE (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], pCppiDesc, SIZE_HOST_DESC);
}
if (ptr_pvt_data->pdi.PhysIdx) {
count = Qmss_getQueueEntryCount (gRxFreeQHnd[0]);
printf ("gRxFreeQHnd[%d] Entry Count: %d\n", 0, count);
}
count = Qmss_getQueueEntryCount (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]);
printf ("gRxFreeQHnd[%d] Entry Count: %d\n", ptr_pvt_data->pdi.PhysIdx, count);
if (i != NIMU_NUM_RX_DESC)
{
printf ("Error allocating Rx free descriptors \n");
return -1;
}
/* Setup a Rx Flow.
*
* A Rx flow encapsulates all relevant data properties that CPDMA would
* have to know in order to successfully receive data.
*/
/* Initialize the flow configuration */
memset (&rxFlowCfg, 0, sizeof(Cppi_RxFlowCfg));
/* Let CPPI pick the next available flow */
rxFlowCfg.flowIdNum = CPPI_PARAM_NOT_SPECIFIED;
rxFlowCfg.rx_dest_qmgr = rxQInfo.qMgr;
rxFlowCfg.rx_dest_qnum = rxQInfo.qNum;
rxFlowCfg.rx_desc_type = Cppi_DescType_HOST;
rxFlowCfg.rx_ps_location = Cppi_PSLoc_PS_IN_DESC;
rxFlowCfg.rx_psinfo_present = 1; /* Enable PS info */
rxFlowCfg.rx_error_handling = 0; /* Drop the packet, do not retry on starvation by default */
rxFlowCfg.rx_einfo_present = 1; /* EPIB info present */
rxFlowCfg.rx_dest_tag_lo_sel = 0; /* Disable tagging */
rxFlowCfg.rx_dest_tag_hi_sel = 0;
rxFlowCfg.rx_src_tag_lo_sel = 0;
rxFlowCfg.rx_src_tag_hi_sel = 0;
rxFlowCfg.rx_size_thresh0_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh1_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh2_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh0 = 0x0;
rxFlowCfg.rx_size_thresh1 = 0x0;
rxFlowCfg.rx_size_thresh2 = 0x0;
rxFlowCfg.rx_fdq0_sz0_qmgr = rxFreeQInfo.qMgr; /* Setup the Receive free queue for the flow */
rxFlowCfg.rx_fdq0_sz0_qnum = rxFreeQInfo.qNum;
rxFlowCfg.rx_fdq0_sz1_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz1_qmgr = 0x0;
rxFlowCfg.rx_fdq0_sz2_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz2_qmgr = 0x0;
rxFlowCfg.rx_fdq0_sz3_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz3_qmgr = 0x0;
rxFlowCfg.rx_fdq1_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq1_qmgr = rxFreeQInfo.qMgr;
rxFlowCfg.rx_fdq2_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq2_qmgr = rxFreeQInfo.qMgr;
rxFlowCfg.rx_fdq3_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq3_qmgr = rxFreeQInfo.qMgr;
/* Configure the Rx flow */
if ((gRxFlowHnd[ptr_pvt_data->pdi.PhysIdx] = Cppi_configureRxFlow (res_mgr_cppi_get_passhandle(), &rxFlowCfg, &isAllocated)) == NULL)
{
printf ("Error configuring Rx flow \n");
return -1;
}
printf("\tgTxFlowHnd=0x%x\n",gRxFlowHnd[ptr_pvt_data->pdi.PhysIdx]);
count = Qmss_getQueueEntryCount (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]);
printf ("gRxFreeQHnd[%d] Entry Count: %d\n", ptr_pvt_data->pdi.PhysIdx, count);
/* All done with Rx configuration. Return success. */
return 0;
}
/** ============================================================================
* @n@b Init_MAC
*
* @b Description
* @n This API initializes the CPGMAC Sliver (MAC Port) port.
*
* @param[in]
* @n macPortNum MAC port number for which the initialization must be done.
*
* @param[in]
* @n macAddress MAC address to configure on this port.
*
* @param[in]
* @n mtu Maximum Frame length to configure on this port.
*
* @return
* @n None
* =============================================================================
*/
Void Init_MAC (uint32_t macPortNum, uint8_t macAddress[6], uint32_t mtu)
{
/* Reset MAC Sliver 0 */
CSL_CPGMAC_SL_resetMac (macPortNum);
while (CSL_CPGMAC_SL_isMACResetDone (macPortNum) != TRUE);
/* Setup the MAC Control Register for this port:
* (1) Enable Full duplex
* (2) Enable GMII
* (3) Enable Gigabit
* (4) Enable External Configuration. This enables
* the "Full duplex" and "Gigabit" settings to be
* controlled externally from SGMII
* (5) Don't Enable any control/error frames
* (6) Enable short frames
*/
CSL_CPGMAC_SL_enableFullDuplex (macPortNum);
CSL_CPGMAC_SL_enableGMII (macPortNum);
CSL_CPGMAC_SL_enableGigabit (macPortNum);
CSL_CPGMAC_SL_enableExtControl (macPortNum);
/* Adding these configurations to allow the switch not to ignore any packets */
CSL_CPGMAC_SL_enableRxCSF(macPortNum);
/* Configure the MAC address for this port */
CSL_CPSW_3GF_setPortMACAddress (macPortNum, macAddress);
/* Configure VLAN ID/CFI/Priority.
*
* For now, we are not using VLANs so just configure them
* to all zeros.
*/
CSL_CPSW_3GF_setPortVlanReg (macPortNum, 0, 0, 0);
/* Configure the Receive Maximum length on this port,
* i.e., the maximum size the port can receive without
* any errors.
*
* Set the Rx Max length to the MTU configured for the
* interface.
*/
CSL_CPGMAC_SL_setRxMaxLen (macPortNum, mtu);
/* Done setting up the MAC port */
return;
}
/** ============================================================================
* @n@b Init_MDIO
*
* @b Description
* @n Not supported at moment. MDIO is not simulated yet.
*
* @param[in]
* @n None
*
* @return
* @n None
* =============================================================================
*/
Void Init_MDIO (Void)
{
/* There is nothing to be done for C6678 EVM */
return;
}
/** ============================================================================
* @n@b Init_Switch
*
* @b Description
* @n This API sets up the ethernet switch subsystem and its Address Lookup
* Engine (ALE) in "Switch" mode.
*
* @param[in]
* @n mtu Maximum Frame length to configure on the switch.
*
* @return
* @n None
* =============================================================================
*/
Void Init_Switch (uint32_t mtu)
{
CSL_CPSW_3GF_PORTSTAT portStatCfg;
uint32_t rx_max_len = mtu + ETHHDR_SIZE + 4; /* 4 bytes of FCS */
/* Enable the CPPI port, i.e., port 0 that does all
* the data streaming in/out of EMAC.
*/
CSL_CPSW_3GF_enablePort0 ();
CSL_CPSW_3GF_disableVlanAware ();
CSL_CPSW_3GF_setPort0VlanReg (0, 0, 0);
CSL_CPSW_3GF_setPort0RxMaxLen (rx_max_len);
/* Enable statistics on both the port groups:
*
* MAC Sliver ports - Port 1, Port 2
* CPPI Port - Port 0
*/
portStatCfg.p0AStatEnable = 1;
portStatCfg.p0BStatEnable = 1;
portStatCfg.p1StatEnable = 1;
portStatCfg.p2StatEnable = 1;
CSL_CPSW_3GF_setPortStatsEnableReg (&portStatCfg);
/* Setup the Address Lookup Engine (ALE) Configuration:
* (1) Enable ALE.
* (2) Clear stale ALE entries.
* (3) Disable VLAN Aware lookups in ALE since
* we are not using VLANs by default.
* (4) No Flow control
* (5) Configure the Unknown VLAN processing
* properties for the switch, i.e., which
* ports to send the packets to.
*/
CSL_CPSW_3GF_enableAle ();
CSL_CPSW_3GF_clearAleTable ();
CSL_CPSW_3GF_disableAleVlanAware ();
CSL_CPSW_3GF_disableAleTxRateLimit ();
/* Setting the Switch MTU Size to more than needed */
CSL_CPGMAC_SL_setRxMaxLen(0, rx_max_len);
CSL_CPGMAC_SL_setRxMaxLen(1, rx_max_len);
//#ifdef SIMULATOR_SUPPORT
CSL_CPSW_3GF_enableAleBypass();
//#endif
/* Done with switch configuration */
return;
}
/** ============================================================================
* @n@b Switch_update_addr
*
* @b Description
* @n This API add/delete entries in the Address Lookup Engine (ALE) in "Switch" mode.
*
* @param[in]
* @n portNum Switch port number.
* @param[in]
* @n macAddress MAC address to configure on the switch.
*
* @param[in]
* @n add 0:add; 1:delete.
*
* @return
* @n None
*
* @Note It supports "add" operation only now.
* =============================================================================
*/
int Switch_update_addr (uint32_t portNum, uint8_t macAddress[6], Uint16 add)
{
CSL_CPSW_3GF_ALE_PORTCONTROL alePortControlCfg;
#ifdef SIMULATOR_SUPPORT
uint32_t i;
CSL_CPSW_3GF_ALE_UNICASTADDR_ENTRY ucastAddrCfg;
#endif
/* Configure the address in "Learning"/"Forward" state */
alePortControlCfg.portState = ALE_PORTSTATE_FORWARD;
alePortControlCfg.dropUntaggedEnable = 0;
alePortControlCfg.vidIngressCheckEnable = 0;
alePortControlCfg.noLearnModeEnable = 0;
alePortControlCfg.mcastLimit = 0;
alePortControlCfg.bcastLimit = 0;
CSL_CPSW_3GF_setAlePortControlReg (portNum, &alePortControlCfg);
#ifdef SIMULATOR_SUPPORT
/* Program the ALE with the MAC address.
*
* The ALE entries determine the switch port to which any
* matching received packet must be forwarded to.
*/
/* Get the next free ALE entry to program */
for (i = 0; i < CSL_CPSW_3GF_NUMALE_ENTRIES; i++)
{
if (CSL_CPSW_3GF_getALEEntryType (i) == ALE_ENTRYTYPE_FREE)
{
/* Found a free entry */
break;
}
}
if (i == CSL_CPSW_3GF_NUMALE_ENTRIES)
{
/* No free ALE entry found. return error. */
return -1;
}
else
{
/* Found a free ALE entry to program our MAC address */
memcpy (ucastAddrCfg.macAddress, macAddress, 6); // Set the MAC address
ucastAddrCfg.ucastType = ALE_UCASTTYPE_UCAST_NOAGE; // Add a permanent unicast address entryALE_UCASTTYPE_UCAST_NOAGE.
ucastAddrCfg.secureEnable = FALSE;
ucastAddrCfg.blockEnable = FALSE;
ucastAddrCfg.portNumber = portNum; // Add the ALE entry for this port
/* Setup the ALE entry for this port's MAC address */
CSL_CPSW_3GF_setAleUnicastAddrEntry (i, &ucastAddrCfg);
}
#endif
/* Done with upading address */
return 0;
}
/** ============================================================================
* @n@b Verify_Init
*
* @b Description
* @n This API initializes the CPPI LLD, opens the PASS CPDMA and opens up
* the Tx, Rx channels required for data transfers.
*
* @param[in]
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Verify_Init (NETIF_DEVICE* ptr_net_device)
{
int32_t count, returnVal = 0, i;
int32_t num_tx_desc = NIMU_NUM_TX_DESC;
int32_t num_rx_desc = NIMU_NUM_RX_DESC;
int32_t max_queue_number = QMSS_MAX_LOW_PRIORITY_QUEUE +
QMSS_MAX_PASS_QUEUE +
QMSS_MAX_LOW_PRIORITY_QUEUE +
QMSS_MAX_PASS_QUEUE +
QMSS_MAX_INTC_QUEUE +
QMSS_MAX_SRIO_QUEUE +
QMSS_MAX_HIGH_PRIORITY_QUEUE +
QMSS_MAX_STARVATION_COUNTER_QUEUE +
QMSS_MAX_INFRASTRUCTURE_QUEUE +
QMSS_MAX_TRAFFIC_SHAPING_QUEUE +
QMSS_MAX_GENERAL_PURPOSE_QUEUE ;
EMAC_DATA *ptr_pvt_data;
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
/*Verify if we got NIMU_NUM_TX_DESC Tx Free Q*/
if ((count = Qmss_getQueueEntryCount (gTxFreeQHnd[ptr_pvt_data->pdi.PhysIdx])) != num_tx_desc) {
printf ("Verify_Init: Expected %d entry count for gTxFreeQHnd queue %d, found %d entries\n", num_tx_desc, gTxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], count);
returnVal = -1;
}
/* Verify if we got NIMU_NUM_RX_DESC Rx FDQ */
if ((count = Qmss_getQueueEntryCount (gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx])) != num_rx_desc) {
printf ("Verify_Init: Expected %d entry count for gRxFreeQHnd queue %d, found %d entries\n", num_rx_desc, gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx], count);
returnVal = -1;
}
/* Verify if we got empty Tx completion Q*/
if ((count = Qmss_getQueueEntryCount (gTxReturnQHnd[ptr_pvt_data->pdi.PhysIdx])) != 0) {
printf ("Verify_Init: Expected 0 entry count for gTxReturnQHnd queue %d, found %d entries\n", gTxReturnQHnd[ptr_pvt_data->pdi.PhysIdx], count);
returnVal = -1;
}
/* Verify if we got NIMU_NUM_RX_DESC Rx FDQ */
if ((count = Qmss_getQueueEntryCount (gRxQHnd[ptr_pvt_data->pdi.PhysIdx])) != 0) {
printf ("Verify_Init: Expected 0 entry count for gRxQHnd= %d, found %d entries\n", gRxQHnd[ptr_pvt_data->pdi.PhysIdx], count);
returnVal = -1;
}
for (i = 0; i < max_queue_number; i++ ) {
if ( (i == gRxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]) || (i == gTxFreeQHnd[ptr_pvt_data->pdi.PhysIdx]) || (i == gTxCmdFreeQHnd[ptr_pvt_data->pdi.PhysIdx]))
continue;
count = Qmss_getQueueEntryCount (i);
if (count != 0) {
printf ("Verify_Init: Expected 0 entry count for Queue number = %d, found %d entries\n", i, count);
}
}
/* Verify_Init Done. Return success */
return (returnVal);
}
/** ============================================================================
* @n@b Init_Cpsw
*
* @b Description
* @n This API sets up the entire ethernet subsystem and all its associated
* components.
*
* @param[in]
* @n None
*
* @return
* @n None
* =============================================================================
*/
int32_t Init_Cpsw (uint32_t mtu, uint8_t* myMACAddress)
{
#ifdef SIMULATOR_SUPPORT
uint8_t bcMACAddress[6] = {0xff,0xff,0xff,0xff,0xff,0xff};
extern uint8_t clientMACAddress [6];
/* Initialize the SGMII/Sliver submodules for the MAC port. */
Init_SGMII (0);
Init_MAC (0, myMACAddress, mtu);
Init_SGMII (1);
Init_MAC (1, myMACAddress, mtu);
/* Setup the Ethernet switch finally. */
Init_Switch (mtu);
/* Update the ALE Entries and ensure that these are correctly configured.
* There are 2 Entries created here:
* Entry1: My OWN MAC Address goes to Port 0
* Entry2: Destination MAC Address is forwarded to Port1
* If there are more destination MAC Addresses to which packets need to be sent
* than additional entries need to be configured. */
/* This is needed only for testing in Simulator*/
Switch_update_addr(0, myMACAddress, 0);
Switch_update_addr(1, clientMACAddress, 0);
Switch_update_addr(1, myMACAddress, 0); // testing a hybrid between cooked up ping and the original app (cooked up raw message)
// checking out if adding bc message still work for unicast
Switch_update_addr(1, bcMACAddress, 0); // verified needed for BCAST tx
// add this to see if BC packet response can come into the PA
Switch_update_addr(0, bcMACAddress, 0); // verfied needed for BCast Rx
#else
uint32_t i;
uint8_t backplaneMac[6] = {0x1, 0x1, 0x1, 0x1, 0x1, 0x1}; /* Mask for creating mac address by flipping LSB */
uint8_t cppiMac [6] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05}; /* MAC address for (CPPI) Port 0 - we made it up*/
/* we need to create a mac address for the Backplane Ethernet port
* using the Ethernet MAC Adress
*/
for (i=0; i < 6; i++) {
backplaneMac[i] |= myMACAddress[i];
}
Init_MAC (0, backplaneMac, mtu);
/* set the silver port to the stacks ethernet address */
Init_MAC (1, myMACAddress, mtu);
/* Setup the Phys by initializing the MDIO - not needed for Simulator*/
Init_MDIO ();
/* Setup the Ethernet switch finally. */
Init_Switch (mtu);
/* This is a little confusing but different APIs use different numbering */
Switch_update_addr(0, cppiMac, 0);
Switch_update_addr(1, backplaneMac, 0);
Switch_update_addr(2, myMACAddress, 0);
#endif
/* CPSW subsystem setup done. Return success */
return 0;
}
/* ============================================================================
* @n@b Init_PASS
*
* @b Description
* @n This API initializes the PASS/PDSP and opens a queue that the application
* can use to receive command responses from the PASS.
*
* @param[in]
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Init_PASS (Void)
{
uint8_t isAllocated;
/* Open a PA Command Response Queue.
*
* This queue will be used to hold responses from the PA PDSP for all the
* commands issued by NIMU.
*
* This queue is used only when configuring the PA PDSP. We will use it when adding our mac address.
*/
if ((gPaCfgCmdRespQHnd = Qmss_queueOpen (Qmss_QueueType_GENERAL_PURPOSE_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
printf ("Error opening a PA Command Response queue \n");
return -1;
}
/* Init done. Return success. */
return 0;
}
/** ============================================================================
* @n@b Add_MACAddress
*
* @b Description
* @n This API adds the switch MAC address to the PA PDSP Lookup table. This
* ensures that all packets destined for this MAC address get processed
* for forwarding to the host.
*
* @param[in]
* @n ethInfo Pointer to PA Ethernet Info table.
*
* @param[in]
* @n routeInfo Pointer to PA Route Info table.
*
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t
Add_MACAddress
(
paEthInfo_t *ethInfo,
paRouteInfo_t *routeInfo
)
{
int32_t j;
uint16_t cmdSize;
Qmss_Queue cmdReplyQInfo;
paRouteInfo_t nFailInfo = { pa_DEST_DISCARD, /* Toss the packet */
0, /* Flow Id = dont care */
0, /* queue = dont care */
0, /* mutli route = dont care */
0, /* swinfo0 = dont care */
0, /* swinfo1 = dont care */
0, /* customType = pa_CUSTOM_TYPE_NONE */ \
0, /* customIndex: not used */ \
0, /* pkyType: for SRIO only */ \
NULL /* No commands */
};
paCmdReply_t cmdReplyInfo = { pa_DEST_HOST, /* Replies go to the host */
0, /* User chosen ID to go to swinfo0 */
0, /* Destination queue */
0 /* Flow ID */
};
paReturn_t retVal;
paEntryHandle_t retHandle;
int32_t handleType, cmdDest;
uint32_t psCmd = ((uint32_t)(4 << 5) << 24);
uint32_t myswinfo[] = {0x11112222, 0x33334444};
uint32_t myswinfo_orig[] = {0x00000000, 0x00000000, 0x00000000};;
uint8_t* pCmdDataBuffer;
Cppi_HostDesc* pHostDesc = NULL;
Qmss_Queue rxQInfo;
uint32_t count, cmdbuf_len = 320;
int32_t ret_val = 0;
int index = 0;
/* If PHY SGMII1, set index to 0 so the queues are indexed in the means they were set up
* in setup_Tx
*/
if (ethInfo->inport == pa_EMAC_PORT_1) {
index = 1;
}
/*If AMC SGMII0, set index to 1 so the queues are indexed in the means they were set up
* in setup_Tx
*/
else if (ethInfo->inport == pa_EMAC_PORT_0) {
index = 0;
}
/* Get a Tx free descriptor to send a command to the PA PDSP */
if ((QMSS_QPOP (gTxCmdFreeQHnd[index], QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc )) != NULL)
{
printf ("Error obtaining a Tx free descriptor \n");
return -1;
}
/* Allocate a Tx buffer and attach the command info to it. */
cmdbuf_len = platform_roundup(cmdbuf_len, PLATFORM_CACHE_LINE_SIZE);
if ((pCmdDataBuffer = (Ptr) Osal_nimuMalloc (cmdbuf_len, PLATFORM_CACHE_LINE_SIZE)) == NULL)
{
printf ("Error allocating memory for PA Command data buffer \n");
return -1;
}
/* Populate the Tx free descriptor with the buffer we just allocated. */
Cppi_setData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)Convert_CoreLocal2GlobalAddr((uint32_t)pCmdDataBuffer), cmdbuf_len);
/* Save original buffer information */
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)Convert_CoreLocal2GlobalAddr((uint32_t)pCmdDataBuffer), cmdbuf_len);
cmdSize = pHostDesc->buffLen;
cmdReplyInfo.replyId = 0x11111111; /* unique for each add mac command */
/* Get the PA response queue number and populate the destination queue number
* in the PA response configuration.
*/
cmdReplyQInfo = Qmss_getQueueNumber (gPaCfgCmdRespQHnd);
cmdReplyInfo.queue = cmdReplyQInfo.qNum;
/* Setup the Rx queue as destination for the packets */
rxQInfo = Qmss_getQueueNumber (gRxQHnd[index]);
routeInfo->queue = rxQInfo.qNum;
retVal = Pa_addMac (res_mgr_get_painstance(),
pa_LUT1_INDEX_NOT_SPECIFIED,
ethInfo,
routeInfo,
&nFailInfo,
&gPaL2Handles[0],
(paCmd_t) pHostDesc->buffPtr,
&cmdSize,
&cmdReplyInfo,
&cmdDest);
if (retVal != pa_OK)
{
printf ("Pa_addMac returned error %d\n", retVal);
ret_val = -1;
goto return_fail;
}
/* This sets the extended info for descriptors, and this is required so PS info
* goes to the right spot
*/
Cppi_setSoftwareInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)myswinfo);
/* Set the buffer length to the size used. It will be restored when the descriptor
* is returned
*/
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, cmdSize);
pHostDesc->buffLen = cmdSize;
/* Mark the packet as a configuration packet */
Cppi_setPSData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)&psCmd, 4);
/* Send the command to the PA and wait for the return */
QMSS_QPUSH (gPaTxQHnd[cmdDest - pa_CMD_TX_DEST_0],
pHostDesc,
pHostDesc->buffLen,
SIZE_HOST_DESC,
Qmss_Location_TAIL
);
/* Poll on the PA response queue to see if response from PA has come */
for (j = 0; j < 100; j++)
{
cpu_delaycycles (1000);
/* Verify if we got empty Tx completion Q*/
count = Qmss_getQueueEntryCount (gTxCmdReturnQHnd[index]);
if (count != 0) {
if ((QMSS_QPOP (gTxCmdReturnQHnd[index], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc)) != NULL)
{
ret_val = -1;
goto return_fail;
}
/* Restore the states */
Cppi_setSoftwareInfo(Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)myswinfo_orig);
Cppi_setPSData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL);
pHostDesc->buffLen = 0;
QMSS_QPUSHDESCSIZE (gTxCmdFreeQHnd[index], pHostDesc, SIZE_HOST_DESC);
}
if (Qmss_getQueueEntryCount (gPaCfgCmdRespQHnd) > 0)
{
/* We have a response from PA PDSP for the command we submitted earlier for
* MAC address addition.
*/
if ((QMSS_QPOP (gPaCfgCmdRespQHnd, QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc)) != NULL)
{
ret_val = -1;
goto return_fail;
}
if (pHostDesc->softwareInfo0 != cmdReplyInfo.replyId)
{
printf ("Found an entry in PA response queue with swinfo0 = 0x%08x, expected 0x%08x\n",
pHostDesc->softwareInfo0, cmdReplyInfo.replyId);
pHostDesc->buffLen = pHostDesc->origBufferLen;
QMSS_QPUSH (gTxCmdFreeQHnd[index], pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
ret_val = -1;
goto return_fail;
}
retVal = Pa_forwardResult (res_mgr_get_painstance(), (Ptr)pHostDesc->buffPtr, &retHandle, &handleType, &cmdDest);
if (retVal != pa_OK)
{
printf ("PA sub-system rejected Pa_addMac command\n");
ret_val = -1;
goto return_fail;
}
/* Reset the buffer length and put the descriptor back on the Rx free queue */
pHostDesc->buffLen = pHostDesc->origBufferLen;
QMSS_QPUSH (gRxFreeQHnd[index], pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
break;
}
}
if (j == 100)
{
printf ("Timeout waiting for reply from PA to Pa_addMac command\n");
Osal_nimuFree (pCmdDataBuffer, cmdbuf_len);
ret_val = -1;
}
return_fail:
Osal_nimuFree (pCmdDataBuffer, cmdbuf_len);
return (ret_val);
}
#define T8_NUM_EXCEPTION_ROUTES 5
#define T8_MAC_BROADCAST_PKT_INDEX 10
#define T8_MAC_MULTICAST_PKT_INDEX 11
#define T8_IP_BROADCAST_PKT_INDEX 12
#define T8_IP_MULTICAST_PKT_INDEX 13
#define T8_CMD_SWINFO0_PKT_ID 0x66660000
static int t8ErouteTypes[] = {
pa_EROUTE_L2L3_FAIL,
pa_EROUTE_MAC_BROADCAST,
pa_EROUTE_MAC_MULTICAST,
pa_EROUTE_IP_BROADCAST,
pa_EROUTE_IP_MULTICAST
};
static paRouteInfo_t t8Eroutes[] = {
/* LUT1 Failure */
{ pa_DEST_EMAC, /* Dest */
0, /* Flow ID */
0, /* queue */
0, /* Multi route */
0, /* sw Info 0 */
0, /* sw Info 1 */
0, /* customType : not used */
0, /* customIndex: not used */
pa_EMAC_CTRL_CRC_DISABLE | pa_EMAC_PORT_NOT_SPECIFIED, /* emacCtrl: for EMAC only */
NULL /* No commands */
},
/* MAC Broadcast */
{ pa_DEST_HOST, /* Dest */
0, /* Flow ID */
0, /* queue */
0, /* Multi route */
T8_MAC_BROADCAST_PKT_INDEX + T8_CMD_SWINFO0_PKT_ID, /* sw Info 0 */
0, /* sw Info 1 */
0, /* customType : not used */
0, /* customIndex: not used */
0, /* pkyType: for SRIO only */
NULL /* No commands */
},
/* MAC Multicast */
{ pa_DEST_HOST, /* Dest */
0, /* Flow ID */
0, /* queue */
10, /* Multi route */
T8_MAC_MULTICAST_PKT_INDEX + T8_CMD_SWINFO0_PKT_ID, /* sw Info 0 */
0, /* sw Info 1 */
0, /* customType : not used */
0, /* customIndex: not used */
0, /* pkyType: for SRIO only */
NULL /* No commands */
},
/* IP Broadcast */
{ pa_DEST_HOST, /* Dest */
0, /* Flow ID */
0, /* queue */
20, /* Multi route */
T8_IP_BROADCAST_PKT_INDEX + T8_CMD_SWINFO0_PKT_ID, /* sw Info 0 */
0, /* sw Info 1 */
0, /* customType : not used */
0, /* customIndex: not used */
0, /* pkyType: for SRIO only */
NULL /* No commands */
},
/* IP Multicast */
{ pa_DEST_HOST, /* Dest */
0, /* Flow ID */
0, /* queue */
31, /* Multi route */
T8_IP_MULTICAST_PKT_INDEX + T8_CMD_SWINFO0_PKT_ID, /* sw Info 0 */
0, /* sw Info 1 */
0, /* customType : not used */
0, /* customIndex: not used */
0, /* pkyType: for SRIO only */
NULL /* No commands */
}
};
int32_t
Add_ExceptionRoute
(
paEthInfo_t *ethInfo,
paRouteInfo_t *routeInfo
)
{
int32_t j;
uint16_t cmdSize;
Qmss_Queue cmdReplyQInfo;
paCmdReply_t cmdReplyInfo = { pa_DEST_HOST, /* Replies go to the host */
0, /* User chosen ID to go to swinfo0 */
0, /* Destination queue */
0 /* Flow ID */
};
paReturn_t retVal;
paEntryHandle_t retHandle;
int32_t handleType, cmdDest;
uint32_t psCmd = ((uint32_t)(4 << 5) << 24);
uint32_t myswinfo[] = {0x11112222, 0x33334444};
uint32_t myswinfo_orig[] = {0x00000000, 0x00000000, 0x00000000};;
uint8_t* pCmdDataBuffer;
Cppi_HostDesc* pHostDesc = NULL;
Qmss_Queue rxQInfo;
uint32_t count, cmdbuf_len = 640;
int32_t ret_val = 0;
int index = 0;
/* If PHY SGMII1, set index to 0 so the queues are indexed in the means they were set up
* in setup_Tx
*/
if (ethInfo->inport == pa_EMAC_PORT_1) {
index = 1;
}
/*If AMC SGMII0, set index to 1 so the queues are indexed in the means they were set up
* in setup_Tx
*/
else if (ethInfo->inport == pa_EMAC_PORT_0) {
index = 0;
}
/* Get a Tx free descriptor to send a command to the PA PDSP */
if ((QMSS_QPOP (gTxCmdFreeQHnd[index], QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc )) != NULL)
{
printf ("Error obtaining a Tx free descriptor \n");
return -1;
}
/* Allocate a Tx buffer and attach the command info to it. */
cmdbuf_len = platform_roundup(cmdbuf_len, PLATFORM_CACHE_LINE_SIZE);
if ((pCmdDataBuffer = (Ptr) Osal_nimuMalloc (cmdbuf_len, PLATFORM_CACHE_LINE_SIZE)) == NULL)
{
printf ("Error allocating memory for PA Command data buffer \n");
return -1;
}
/* Populate the Tx free descriptor with the buffer we just allocated. */
Cppi_setData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)Convert_CoreLocal2GlobalAddr((uint32_t)pCmdDataBuffer), cmdbuf_len);
/* Save original buffer information */
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)Convert_CoreLocal2GlobalAddr((uint32_t)pCmdDataBuffer), cmdbuf_len);
cmdSize = pHostDesc->buffLen;
cmdReplyInfo.replyId = 0x44440000; /* unique for each add mac command */
/* Get the PA response queue number and populate the destination queue number
* in the PA response configuration.
*/
cmdReplyQInfo = Qmss_getQueueNumber (gPaCfgCmdRespQHnd);
cmdReplyInfo.queue = cmdReplyQInfo.qNum;
/* Setup the Rx queue as destination for the packets */
rxQInfo = Qmss_getQueueNumber (gRxQHnd[index]);
routeInfo->queue = rxQInfo.qNum;
retVal = Pa_configExceptionRoute (res_mgr_get_painstance(),
T8_NUM_EXCEPTION_ROUTES,
t8ErouteTypes,
t8Eroutes,
(paCmd_t) pHostDesc->buffPtr,
&cmdSize,
&cmdReplyInfo,
&cmdDest);
if (retVal != pa_OK)
{
printf ("Pa_configExceptionRoute returned error %d\n", retVal);
ret_val = -1;
goto return_fail;
}
/* This sets the extended info for descriptors, and this is required so PS info
* goes to the right spot
*/
Cppi_setSoftwareInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)myswinfo);
/* Set the buffer length to the size used. It will be restored when the descriptor
* is returned
*/
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, cmdSize);
pHostDesc->buffLen = cmdSize;
/* Mark the packet as a configuration packet */
Cppi_setPSData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)&psCmd, 4);
/* Send the command to the PA and wait for the return */
QMSS_QPUSH (gPaTxQHnd[cmdDest - pa_CMD_TX_DEST_0],
pHostDesc,
pHostDesc->buffLen,
SIZE_HOST_DESC,
Qmss_Location_TAIL
);
/* Poll on the PA response queue to see if response from PA has come */
for (j = 0; j < 100; j++)
{
cpu_delaycycles (1000);
/* Verify if we got empty Tx completion Q*/
count = Qmss_getQueueEntryCount (gTxCmdReturnQHnd[index]);
if (count != 0) {
if ((QMSS_QPOP (gTxCmdReturnQHnd[index], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc)) != NULL)
{
ret_val = -1;
goto return_fail;
}
/* Restore the states */
Cppi_setSoftwareInfo(Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)myswinfo_orig);
Cppi_setPSData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL);
pHostDesc->buffLen = 0;
QMSS_QPUSHDESCSIZE (gTxCmdFreeQHnd[index], pHostDesc, SIZE_HOST_DESC);
}
if (Qmss_getQueueEntryCount (gPaCfgCmdRespQHnd) > 0)
{
/* We have a response from PA PDSP for the command we submitted earlier for
* MAC address addition.
*/
if ((QMSS_QPOP (gPaCfgCmdRespQHnd, QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc)) != NULL)
{
ret_val = -1;
goto return_fail;
}
if (pHostDesc->softwareInfo0 != cmdReplyInfo.replyId)
{
printf ("Found an entry in PA response queue with swinfo0 = 0x%08x, expected 0x%08x\n",
pHostDesc->softwareInfo0, cmdReplyInfo.replyId);
pHostDesc->buffLen = pHostDesc->origBufferLen;
QMSS_QPUSH (gTxCmdFreeQHnd[index], pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
ret_val = -1;
goto return_fail;
}
retVal = Pa_forwardResult (res_mgr_get_painstance(), (Ptr)pHostDesc->buffPtr, &retHandle, &handleType, &cmdDest);
if (retVal != pa_OK)
{
printf ("PA sub-system rejected Pa_addMac command\n");
ret_val = -1;
goto return_fail;
}
/* Reset the buffer length and put the descriptor back on the Rx free queue */
pHostDesc->buffLen = pHostDesc->origBufferLen;
QMSS_QPUSH (gRxFreeQHnd[index], pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
break;
}
}
if (j == 100)
{
printf ("Timeout waiting for reply from PA to Add_ExceptionRoute command\n");
Osal_nimuFree (pCmdDataBuffer, cmdbuf_len);
ret_val = -1;
} else {
printf ("Add_ExceptionRoute command successfully!\n");
}
return_fail:
Osal_nimuFree (pCmdDataBuffer, cmdbuf_len);
return (ret_val);
}
/**
* @b Description
* @n
* Returns the number of received packet drops, most likely due to NDK buffer starvation.
*
* @retval
* None.
*/
uint32_t nimu_getrxdrops(void) {
return gRxDropCounter;
}
/**
* @b Description
* @n
* Returns the number of transmit packet drops due to Tx descriptor starvation.
*
* @retval
* None.
*/
uint32_t nimu_gettxdrops(void) {
return gTxDropCounter;
}
#ifdef TIMING
/*
* Routine to print out timing measurements.. meant to be called from application as we dont
* want to print in an interrupt context.
*/
void print_nimu_timing(void) {
uint32_t avg_rxisr, avg_txisr, max_rxisr, min_rxisr, max_txisr, min_txisr;
uint32_t total_rx, total_tx;
uint32_t i, x, n;
void* key;
/* Begin Critical Section before accessing shared resources. */
key = Osal_qmssCsEnter ();
/* Calculate min, max, avg times for display */
avg_rxisr = 0;
avg_txisr = 0;
max_rxisr = 0;
min_rxisr = (uint32_t) (rxisr_time[0]); /* seed the value */
max_txisr = 0;
min_txisr = (uint32_t) (txisr_time[0]); /* seed the value */
total_rx = 0;
total_tx = 0;
for (i=0, n=0; i < MAX_TIMING_PACKETS; i++) {
x = (uint32_t) (rxisr_time[i]);
if (rxisr_time[i] != 0) {
n++;
if (min_rxisr > x) {
min_rxisr = x;
}
if ( max_rxisr < x) {
max_rxisr = x;
}
total_rx += x;
}
x = (uint32_t) (txisr_time[i]);
if (txisr_time[i] != 0) {
if ( min_txisr > x && x > 0) {
min_txisr = x;
}
if ( max_txisr < x) {
max_txisr = x;
}
total_tx += x;
}
}
/* End Critical Section */
Osal_qmssCsExit (key);
avg_rxisr = total_rx / n; /* have to avg over number of times it was called */
avg_txisr = total_tx / MAX_TIMING_PACKETS;
printf ("NIMU Rx (%d Packets): Total = %d Min = %d Max = %d Avg = %d \n", MAX_TIMING_PACKETS, total_rx, min_rxisr, max_rxisr, avg_rxisr);
printf ("NIMU Tx (%d Packets): Total = %d Min = %d Max = %d Avg = %d \n", MAX_TIMING_PACKETS, total_tx, min_txisr, max_txisr, avg_txisr);
}
/* reset timing counters */
void reset_nimu_timing(void) {
void* key;
/* Begin Critical Section before accessing shared resources. */
key = Osal_qmssCsEnter ();
memset (&rxisr_time[0], 0, MAX_TIMING_PACKETS);
memset (&txisr_time[0], 0, MAX_TIMING_PACKETS);
rxisr_time_idx = 0; txisr_time_idx = 0;
rxisr_pktcount = 0;
/* End Critical Section */
Osal_qmssCsExit (key);
}
#endif
/* Nothing past this point */