Part Number: AM6442
Other Parts Discussed in Thread: TMDS64EVM, UNIFLASH
Hi,
I have a TMDS64EVm board which is an HS-FS device.
I was able to run the hello_world example on it. For that I first put it in UART boot mode, flashed the sbl_null, and then put it in OSPI boot mode and programmed the hello world example on it through CCS.
Now I would like to be able to use the Lauterbach debugger. However, the connection fails. The script fails after "System.up" which means that the connection fails.
I have tried both of the CMMS for DDR as well as SRAM.
Is there any specific configuration that needs to be done before using Lauterbach?
Thanks,
Boshra