Part Number: AM623
Other Parts Discussed in Thread: SK-AM62,
Hi team,
My customer want to know if Am623 support USB DFU boot mode without translating to UART(SK-AM62). If yes, could you provide which part in TRM has this content, thanks!


BR
Sirui
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sirui,
support USB DFU boot mode without translating to UART
I am not sure I understand your question. Could you please elaborate?
Please also check if the following instruction answers your question:
Hi Bin
I want to booting with USB DFU in windows OS.
I tried to follow this document, but there was an error in the second step.like picture 1

Do I need to use am62x_ Evm_ R5_ Usbdfu_ Defconfig and am62x_ Evm_ A53_ Defconfig Reconfiguration?

Hi Linmaoyuping,
Are you working with Sirui together on the same issue as Sirui reported above?
Hi linmaoyuqing,
Do I need to use am62x_ Evm_ R5_ Usbdfu_ Defconfig and am62x_ Evm_ A53_ Defconfig Reconfiguration?
Yes, when using DFU mode, the U-Boot binaries have to be recompiled using the mentioned defconfig. Otherwise, the DFU function in U-Boot is not enabled.