Part Number: TDA4VM
Hi team,
SDK: Processor SDK Linux for J721e 08_06_01
The compilation is complete and burned to the SD to enter the system and the customer is currently planning to add layer.
$ cd /ti-processor-sdk-linux-j7-evm-08_06_01_02/yocto-build
$ . ./sources/oe-core/oe-init-build-env
$ bitbake-layers create-layer meta-stressapptest
However, the problem occurs as shown in the following figure:

They then tried to modify toolchain_base_path, but because of the lack of GCC-arm-9.2-ti2020.01-armv5-x86_64-arm-none-Linux-gnueabi, the new meta-stringapptest cannot be generated.

NOTE: Starting bitbake server...
ERROR: Unable to start bitbake server (None)
ERROR: Server log for this session (/home/macon/works/jacinto7/j721e_evm/linux/20230521_08_06_01_02/ti-processor-sdk-linux-j7-evm-08_06_01_02/yocto-build/build/bitbake-cookerdaemon.log):
--- Starting bitbake server pid 3440 at 2023-06-06 17:06:14.944751 ---
ERROR: Failed to obtain external Arm toolchain version: Execution of '/home/macon/works/jacinto7/toolchain/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -v' failed: command not found
--------
According to doc, only 2 toolchains are required:
gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu.tar.xz
gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf.tar.xz
1) Is it possible to remove the GCC-arm-9.2-ti2020.01-armv5-x86_64-arm-none-Linux-gnueabi requirement? If so, how to modify it?
2) If not, where can they download gcc-arm-9.2-ti2020.01-armV5-x86_64-arm-none-Linux-gnueab?
Could you help check this case? Thanks.
Best Regards,
Cherry