Hello,
Table 6-1, Input Requirements for Crystal on the 32.768-kHz RTC Oscillator, of SPRS660D indicates the maximum crystal drive is 1.0 uW. Is this a requirement for the crystal, or is it a characteristic of the DSP's RTC oscillator? In other words, does the crystal need to be able to dissipate at least 1uW? If so, it might be worthwhile to update the table to separate the items which are xtal requirements and those which are DSP characteristics.
Thanks - AM