This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Does TDA4 uboot support bootcount?

Genius 13655 points

Part Number: TDA4VM

Hello Champs,

SDK:08_00_06_11

uboot:u-boot-2021.01+gitAUTOINC+62a9e51344-g62a9e51344


Customer is developing TDA4 uboot which is related with bootcount. He found that the CONFIG_BOOTCOUNT_LIMIT is not supported in j721E.

Does TDA4 uboot support bootcount? If not, is there some other scheme available?

Thanks
Regards
Shine

  • Customer is developing TDA4 uboot which is related with bootcount. He found that the CONFIG_BOOTCOUNT_LIMIT is not supported in j721E.

    Does TDA4 uboot support bootcount? If not, is there some other scheme available?

    There is NO support for this as observed by the customer. Can you elaborate on the customer's requirement?

    - Keerthy