Part Number: TDA4VM
Other Parts Discussed in Thread: ADS8684
Hi team,
The SDK version is ti-processor-SDK-Linux-J7-EVM-08_05_00_08-Linux, the ADC being used is ADS8684.
Refer to software-dl.ti.com/.../iio:device0 to see the corresponding file and get the value of the corresponding file for the channel. However, when setting the continuous read mode, it can be set successfully before, and finally it cannot be set successfully at echo 1 > /sys/bus/iio/devices/iio\:device0/buffer/enable, and it will prompt "-sh: echo: write error: Invalid argument".
Could you help check this case? Thanks.
Best Regards,
Cherry