Hi,
We have a few related questions on I2C features on the J7 family, relating to the TRM:
RX and TX FIFOs depth can be checked in I2C_BUFSTAT[15-14]FIFODEPTH:
- How FIFOs depth value is determined ? Is it a constant value depending on a hardware version or does it depends on FIFOs Thresholds programmed values ?
DMA mode and SCCB Protocol are not supported on this family of device: However §12.1.3.3.7.3 I2C Draining Feature mention DMA transfers in most of the given examples.
- Does that mean that draining feature is only available with DMA included hardware version (so not J784S4) or that DMA transfers examples can be occulted from this chapter ?