Part Number: AM3358
Hi,
Can we use AM335x PRU ethernet module for purpose of verifying preamble and SFD of ethernet Rx frame on PRU ethernet interface?
Also, can we change number of preamble bytes send in Tx frame from AM335x PRU MAC?
Could we send an Ethernet Frame with TX_ER asserted from this PRU MAC to the PHY to see if the link partner responds with RX_ER?
Referring to technical document spruh73q, i believe we can be able to achieve above requirement. Request to confirm.
Can you suggest which TI SDK and PRU driver to be used and if any documentation for it on 10Mbps and 100Mbps? Thanks!
Regards,
Dave