Part Number: TDA4VH-Q1
Hi team,
In the sdk8.6 platform, the sgmii phy of 2-0 is debugged in rtos, which requires configuration of sgmii and serdes:
serdes1 lane 1
serdes 2 lane 0 1 2 3 4


But PLL errors occur during the process:
CpswMacPort_setSgmiiInterface: MAC 4: SERDES PLL is not locked
[MCU2_0] 17.794998 s: EnetMcm: CPSW_9G on MAIN NAVSS
[MCU2_0] 17.810964 s: PHY 0 is no alive
[MCU2_0] 17.811022 s: PHY 1 is no alive
[MCU2_0] 17.811053 s: PHY 2 is alive
[MCU2_0] 17.811080 s: PHY 3 is no alive
[MCU2_0] 17.811107 s: PHY 4 is no alive
[MCU2_0] 17.811135 s: PHY 5 is no alive
[MCU2_0] 17.811161 s: PHY 6 is no alive
[MCU2_0] 17.811187 s: PHY 7 is no alive
[MCU2_0] 17.811214 s: PHY 8 is no alive
[MCU2_0] 17.811241 s: PHY 9 is no alive
[MCU2_0] 17.811267 s: PHY 10 is no alive
[MCU2_0] 17.811295 s: PHY 11 is no alive
[MCU2_0] 17.811323 s: PHY 12 is no alive
[MCU2_0] 17.811350 s: PHY 13 is no alive
[MCU2_0] 17.811377 s: PHY 14 is no alive
[MCU2_0] 17.811404 s: PHY 15 is no alive
[MCU2_0] 17.811432 s: PHY 16 is no alive
[MCU2_0] 17.811459 s: PHY 17 is no alive
[MCU2_0] 17.811486 s: PHY 18 is no alive
[MCU2_0] 17.811513 s: PHY 19 is no alive
[MCU2_0] 17.811547 s: PHY 20 is no alive
[MCU2_0] 17.811575 s: PHY 21 is no alive
[MCU2_0] 17.811601 s: PHY 22 is no alive
[MCU2_0] 17.811627 s: PHY 23 is no alive
[MCU2_0] 17.811654 s: PHY 24 is no alive
[MCU2_0] 17.811681 s: PHY 25 is no alive
[MCU2_0] 17.811707 s: PHY 26 is no alive
[MCU2_0] 17.811734 s: PHY 27 is no alive
[MCU2_0] 17.811760 s: PHY 28 is no alive
[MCU2_0] 17.811787 s: PHY 29 is no alive
[MCU2_0] 17.811813 s: PHY 30 is no alive
[MCU2_0] 17.811846 s: EnetMcm_enablePorts() +to open MAC port: 3
[MCU2_0] 17.812042 s: CpswMacPort_setSgmiiInterface: MAC 4: SERDES PLL is not locked 0x0
[MCU2_0] 17.812078 s: CpswMacPort_setSgmiiInterface:
[MCU2_0] 17.812113 s: Assertion @ Line: 2201 in src/mod/cpsw_macport.c: false
{
/* Configure SerDes clocks */
EthFwBoard_configTorrentClks();
/* Configure SerDes for QSGMII functionality */
boardStatus = Board_serdesCfgSgmii();
EnetAppUtils_assert(boardStatus == BOARD_SOK);
boardStatus = Board_serdesCfgSgmii_serdes1();
// EnetAppUtils_assert(boardStatus == BOARD_SOK);
Board_STATUS Board_CfgSgmii_serdes1(void)
{
CSL_SerdesResult result;
CSL_SerdesLaneEnableStatus laneRetVal = CSL_SERDES_LANE_ENABLE_NO_ERR;
CSL_SerdesLaneEnableParams serdesLane0EnableParams = {0};
printf("%s %d \n",__func__,__LINE__);
memset(&serdesLane0EnableParams, 0, sizeof(serdesLane0EnableParams));
/* SGMII Config */
serdesLane0EnableParams.serdesInstance = (CSL_SerdesInstance)CSL_TORRENT_SERDES1;
serdesLane0EnableParams.baseAddr = CSL_WIZ16B8M4CT3_1_WIZ16B8M4CT3_BASE;
serdesLane0EnableParams.refClock = CSL_SERDES_REF_CLOCK_100M;
serdesLane0EnableParams.refClkSrc = CSL_SERDES_REF_CLOCK_INT1;
serdesLane0EnableParams.linkRate = CSL_SERDES_LINK_RATE_1p25G;
serdesLane0EnableParams.numLanes = 0x2;
serdesLane0EnableParams.laneMask = 0x4;
serdesLane0EnableParams.SSC_mode = CSL_SERDES_NO_SSC;
serdesLane0EnableParams.phyType = CSL_SERDES_PHY_TYPE_SGMII;
serdesLane0EnableParams.operatingMode = CSL_SERDES_FUNCTIONAL_MODE;
serdesLane0EnableParams.phyInstanceNum = BOARD_SERDES_LANE_SELECT_CPSW;
serdesLane0EnableParams.pcieGenType = CSL_SERDES_PCIE_GEN3;
serdesLane0EnableParams.laneCtrlRate[0] = CSL_SERDES_LANE_FULL_RATE;
serdesLane0EnableParams.loopbackMode[0] = CSL_SERDES_LOOPBACK_DISABLED;
serdesLane0EnableParams.laneCtrlRate[1] = CSL_SERDES_LANE_FULL_RATE;
serdesLane0EnableParams.loopbackMode[1] = CSL_SERDES_LOOPBACK_DISABLED;
CSL_serdesPorReset(serdesLane0EnableParams.baseAddr);
/* Select the IP type, IP instance num, Serdes Lane Number */
CSL_serdesIPSelect(CSL_CTRL_MMR0_CFG0_BASE,
serdesLane0EnableParams.phyType,
serdesLane0EnableParams.phyInstanceNum,
serdesLane0EnableParams.serdesInstance,
1U);
result = CSL_serdesRefclkSel(CSL_CTRL_MMR0_CFG0_BASE,
serdesLane0EnableParams.baseAddr,
serdesLane0EnableParams.refClock,
serdesLane0EnableParams.refClkSrc,
serdesLane0EnableParams.serdesInstance,
serdesLane0EnableParams.phyType);
if (result != CSL_SERDES_NO_ERR)
{
return BOARD_FAIL;
}
/* Assert PHY reset and disable all lanes */
CSL_serdesDisablePllAndLanes(serdesLane0EnableParams.baseAddr, serdesLane0EnableParams.numLanes, serdesLane0EnableParams.laneMask);
/* Load the Serdes Config File */
result = CSL_serdesEthernetInit(&serdesLane0EnableParams);
/* Return error if input params are invalid */
if (result != CSL_SERDES_NO_ERR)
{
return BOARD_FAIL;
}
/* Common Lane Enable API for lane enable, pll enable etc */
laneRetVal = CSL_serdesLaneEnable(&serdesLane0EnableParams);
if (laneRetVal != 0)
{
return BOARD_FAIL;
}
return BOARD_SOK;
}
According to the print, it seems like the 2-0 is stuck.
Board_ethConfigCpsw9g 663
[MCU2_0] 61.678121 s: Board_CfgSgmii_serdes1 393
[MCU2_1] 47.263577 s: CIO: Init ... Done !!!
[MCU2_1] 47.263628 s: ### CPU Frequency = 1000000000 Hz
[MCU2_1] 47.263661 s: CPU is running FreeRTOS
[MCU2_1] 47.263681 s: APP: Init ... !!!
[MCU2_1] 47.263700 s: SCICLIENT: Init ... !!!
[MCU2_1] 47.263865 s: SCICLIENT: DMSC FW version [8.6.3--v08.06.03 (Chill Capybar]
[MCU2_1] 47.263899 s: SCICLIENT: DMSC FW revision 0x8
The customer would like to know how to configure the sgmii and serdes needed in the schematic and make sure they are working? Thanks.
Best Regards,
Cherry