Part Number: AM5718
Other Parts Discussed in Thread: AM6442
Hi,
I am working 0n AM5718. I want to know that it is possible to implement baremetal on am5718.If possible can you guide how can i do that in detail.
Like,
1) Is there any procedure that explains that i can work with baremetal in am5718?
if i can
1)how can i load the code into am5718?
2)In which device should i load the load i.e, either internal flash or external flash?
Thanks & regards,
Bhardwaj.