Other Parts Discussed in Thread: DM3730
Hi all
I have some questions of this. I used the SIM5218 module to connect DM3730.It can call and send message, sometimes i surf the web ,the device would disconnect but sometimes not .It printed:
hub 1-0:1.0: port 2 disabled by hub (EMI?), re-enabling...
usb 1-2: USB disconnect, address 2
generic ttyUSB0: generic converter now disconnected from ttyUSB0
usbserial_generic 1-2:1.0: device disconnected
generic ttyUSB1: generic converter now disconnected from ttyUSB1
usbserial_generic 1-2:1.1: device disconnected
generic ttyUSB2: generic converter now disconnected from ttyUSB2
usbserial_generic 1-2:1.2: device disconnected
generic ttyUSB3: generic converter now disconnected from ttyUSB3
usbserial_generic 1-2:1.3: device disconnected
generic ttyUSB4: generic converter now disconnected from ttyUSB4
usbserial_generic 1-2:1.4: device disconnected
usb 1-2: new high speed USB device using ehci-omap and address 3
select 1171 (droid.bluetooth), adj 15, size 4219, to kill
send sigkill to 1171 (droid.bluetooth), adj 15, size 4219
usb 1-2: device descriptor read/64, error -110
The kernel :
Device Drivers--->
[*]Network
device support--->
<M> PPP (point-to-point
protocol)Support
[]PPP multilink support (EXPERIMENTAL)
[]PPP filtering
<*>PPP support for async serial
ports
<*>PPP support for sync tty
ports
<*>PPP Deflate compression
<* >PPP BSD-Compress compression
< *>PPP MPPE compression (encryption)
(EXPERIMENTAL)
<*>PPP over Ethernet
(EXPERIMENTAL)
<*>PPP over ATM
<*>PPP over L2TP (EXPERIMENTAL)
[*]USB
support--->
<*>USB Serial Converter support--->
<*> USB Generic Serial Driver
<*>USB driver for GSM and CDMA modems