Hello, I am trying to boot AM/DM37X Sitara board from NFS using
I am using the following url to prepare rootfs, and put the rootfs to the exported nfs directory. http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_DeveloperGuide http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_UserGuide I am bit confused with <<<mpurate=1000/720, mem=68M@0x80000000 mem=128M@0x88000000 mem=128M, mem=256M >>etc information I got from http://code.google.com/p/rowboat/wiki/DSP The kernel bootargs from google and TI are not in sync. What should be the correct bootargs I need to pass to the kernel. I got kernel panic, here is the attached l3276.kernel_panic.txtog for kernel panic.
Request your help pls. --Batsayan Das