Part Number: TDA4VM
Hi team,
SDK: ti-processor-sdk-linux-j7-evm-08_05_00_08 + ti-processor-sdk-rtos-j721e-evm-08_05_00_11
Application scenario: Max96724, 4 camera CSI_RX input -- this section is turned on. According to the manual, CSI_TX can receive data in memory through stream0, as shown in the following figure:

4-way camera images received by CSI_RX are fused in memory through a node and then output to CSI_TX (4-way image resolution reduced, 1080p resolution combined). Is this approach possible? And is there a routine available for reference from stream0 input and then from CSI_TX output?
Could you help check this case? Thanks.
Best Regards,
Cherry