Part Number: TDA4VM
Hi team,
1) A mainframe production project where customers want to deploy solid-state laser model pointpillar net on the TDA4VM plus.
According to the TIDL user manual, only 26 calculus are supported and the tensor requirement entered is either RGB or BGR. Does the model deployment tool that comes with this processor, tidl, support point cloud input, scatternd arithmetic, and custom calculations?

...

2) Use the pointpillar onnx model provided by the official github. Is there a txt configuration file for the model to be used for reference?
3) TI deep Learning Product User Guide->TIDL-RT Importer: What is the form of inWidth /inHeight / inNumber for multiple input tensors? String? Separate with commas or spaces?
4) TI deep Learning Product User Guide->TIDL-RT Importer: What form is used as input in the list file for quantifying inData? And how to quantify other parameters? How much quantity of the quantized sample would be appropriate?
5) The TI deep Learning Library User Guide->TIDL Input and Output sensors Format mentions that the input sensor is 3 channels. Uchar ushort type, does it mean that more than 3 channels or floats are not supported?
Could you help check this case? Thanks.
Best Regards,
Cherry