This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Two video cameras on DM6437

Hello,

We are planning to develop some stereo-vision based applications by using a DM6437 EVM. However, I am not sure if it is possible to connect two cameras to his board. And if so, how it can be done? what kind of cameras are better? ip-cameras, analog,...? Did anybody try to do that?

Thanks in advance,

David

  • Dvid,

           Stereo -vision applications are not possible on DM6437 EVM because of only one video input challel on EVM. You can build up your own board with two input channels, such as decorders.

    best regards,

    Dabo Guo