Hi,
I have two questions about the power up sequence related to TMS320VC5509A on the board.
1) Is there a power-up sequence requirment about the I/O voltage DVDD and Core voltage CVDD?
2), On our board there is one 1.8V voltage source which is connected to 5509A's ADC input port for monitoring. This 1.8V is powered up earlier or at the same time of DVDD and CVDD. Is this a risk to C5509A as ADC input is driven before its DVDD and CVDD are well powered up?
BTW: I haven't found any description about these two situations in the datasheet and application notes.
Thanks,