I am reading the Documents comes with the TI J721e SDK.. and there it reads at section 3.2.2.10.3.2.3.2.5. Switch Mode
Quote: All the SoCs listed above support Switch Mode when configured in QSGMII mode.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Quote: All the SoCs listed above support Switch Mode when configured in QSGMII mode.
Hi,
Does this implies that all the 9port switch ethernet phy has to be wired in QSGMII mode in order to use Native Driver in SWITCH MODE?
No, Switch mode enable is independent of MAC Interface.
You can enable switch mode in Native Driver irrespective of phy interface.
Above could be a documentation issue, will correct it.
Best Regards,
Sudheer