This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 multiple rank



1) In the DSP C6-INTEGRA is possible connect to an EMIF port four chip DDR3 of type 16Mx16x8 banks two on DDR{x}_CS[0] and the other two on DDR{x}_CS[1] ( 2 ranks)?

2)The first 512B of HVDPSS is useful from other system component like normal memory space?Is this an extra RAM, different from EMIF0/1? Where is connected?

Thank you

Luca

  • Luca,

    Please refer to the table of Supported DDR3 Device Combinations in the device datasheet.  We are only supporting one CS because it has improved margins, and a second CS is not needed to fully populate the memory space available in the device memory map for DDR3.

    Regards,
    Marc