All of the documentation available recommends a 45.3 ohm resistor on the PTV15 pin.
I'm working on a design that already utilizes a 22 ohm resistor.
I had problem what not booting DDR3. but After replacing the 45.3 ohm with 22 ohm, all the boards DDR3 can work now.
so I had question to you..
question 1 : Can I use a resistor other than 45.3 ohm in PTV15 pin of TMS320C6678 ?
question 2 : Any idea how a 45 ohm resistor would alter the driver?
below eval module has a note showing, The reason why I used other resistor.
* DDR3 Drive Strength - TMDXEVM6678L_EVM_A101-1_DSN, 13 page DSP_DDR3(DSPM-8301E, Rev. A101-1)
70 ohm: 6mA
60 ohm: 7mA
50 ohm: 8mA
45 ohm: 9mA
40 ohm: 10mA
36 ohm: 11mA
That's the only reference I can find to adjusting the value beyond the 45.3 ohms documented elsewhere.