Part Number: AM68A
Other Parts Discussed in Thread: SK-AM68, AM68
Hi TI
There'e three questions while customer review PCB Fabriction Note attached below.
[Q1] The note contains information about BACK DRILL (17. Backdrilling to be done from L12 to L04).
There are 16 NETs using 4 Layer to 12 Layer BACKDRILL, not on the AM68A SoC side, only on the bottom of LPDDR4.
DDR0_CA0~DDR1_CA5, DDR0_CK_T,DDR0_CK_C : LPDDR4 0 : 8ea Nets
DDR1_CA0~DDR1_CA5, DDR1_CK_T,DDR1_CK_C : LPDDR4 1 : 8ea Nets
Please check if the BACK DRILLING work of the NETs must be carried out.
[Q2] 2. Also, there is no clear mention of PCB material in Fabrication Note.
Is it possible to make a PCB with FR4? Or please check if I should use a PCB with a special material.
[Q3] 3. I cannot download AM68A SoC's DESIGN GUIDE from the homepage (ti.com ).
Please deliver the PCB Design Guide data for AM68A SoC.
I am only able to see the following docus.
* Jacinto 7 LPDDR4 Board Design and Layout Guidelines (Rev. E)
* Jacinto 7 High-Speed Interface Layout Guidelines
Thanks
Best Regards,
Jack