This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM:A72 linear decrease in total memory during aging

Part Number: TDA4VM

HI  expert

          Our two applications mainly use CAMERA and C7X resources. After aging for 3 hours,/proc/meminfo recorded a decrease in memory. After 8 hours, the memory ran out, and when the process was killed, the memory returned to normal.

软件运行2.2小时后,X开始线性增长,运行10小时左右内存不足导致node1退出;整个过程中,各进程内存无明显增长;

                                  多次测试发现X开始增长的时间基本一直,都在运行后的2.2小时左右

                                  通过屏蔽模块,只启动eda+行车(DataSource+侧视)时,X也会在运行2.2h后开始增长

 X计算公式有以下公式推出:MemTotal = MemFree +【Slab+ VmallocUsed + PageTables + KernelStack + HardwareCorrupted + Bounce + X】+【Active + Inactive + Unevictable + (HugePages_Total * Hugepagesize)】