Part Number: TDA4VM
Other Parts Discussed in Thread: SYSCONFIG, SYSBIOS
Hi team,
SDK: Processor SDK RTOS J721E 08_06_01
There is no problem with build and Run to flash to the micro SD card using Video Apps previously.
1) Does the current SDK RTOS primarily want to use make to build bin files for co-processes development? If the customer want to develop Main Domain - R5F, just to modify the demo code directly to speed up the development process? As shown below "platform/${SOC}/rtos", or which path needs to be developed first?

2) Should Video Apps be the primary development principal architecture location? To develop MCUSW, is it required to port relevant information to Video Apps? Or use the bin developed by MCUSW to put in Video Apps?
3) CCS is primarily used as a debug tool? Each coprocessor can be created in CCS and the entire chip can be configured in sysconfig. But the RTOS is not available since it required to import other SDK?
4) Is it recommended to review the documentation for the MCU side development process first?
Could you help check this case? Thanks.
Best Regards,
Cherry